Part Number: TDA4VL-Q1
Other Parts Discussed in Thread: TDA4VL
Tool/software:
hello,I have a project using TDA4VL's SOC, SDK version is 8.5, and an exception occurs during IPC initialization, which can be stably reproduced..Please help us investigate the cause.
The log printed by the SOC in normal use is as follows

The log of abnormal SOC is as follows:

As shown in the figure above, MCU2_0 runs to (IPC: HLOS is ready !!!) and then stops.
The code that needs to be run afterwards is as follows