This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello ti,
I am trying to add the below opencv packages in the build :
- opencv_dnn_objdetect
-opencv_dnn_superres
- opencv_freetype
- opencv_hdf
- opencv_text
- opencv_viz
Please suggest me how do I add it my build, do I need to include any specific layer or the recipe for the same.
I am using am62ax processor SDK - build version 9.02
When you review the OpenCV recipe at meta-openembedded/meta-oe/recipes-support/opencv/opencv_* you'll see that at least some of the packages you want are referenced in the PACKAGECONFIG[] object. To activate those features you need to add what's needed to the PACKAGECONFIG variable, see https://docs.yoctoproject.org/ref-manual/variables.html#term-PACKAGECONFIG
Regards, Andreas
Hello Andreas,
Thanks for the support, got most of the packages included but now I am getting the below error :
"Rebuild the library with Windows, GTK+ 2.x or Cocoa support. If you are on Ubuntu or Debian, install libgtk2.0-dev and pkg-config, then re-run cmake or configure script in function 'cvShowImage'"
How do I add support for libgtk2.0 in the build.
Hi Monica,
"Rebuild the library with Windows, GTK+ 2.x or Cocoa support. If you are on Ubuntu or Debian, install libgtk2.0-dev and pkg-config, then re-run cmake or configure script in function 'cvShowImage'"
I suppose this error the result of adding one of the OpenCV packages?
How do I add support for libgtk2.0 in the build.
Looks like there's a recipe that can provide this library, located at meta-openembedded/meta-oe/recipes-gnome/gtk+/gtk+_2.24.33.bb.
You could experiment with adding...
DEPENDS = "gtk+"
or
RDEPENDS:${PN} = "gtk+"
To your OpenCV recipe.
Regards, Andreas
The recipe is there but it can't be build during missing distro features, as the error message states. This is caused by this line here:
oe-core/meta/conf/distro/include/default-distrovars.inc:GTK2DISTROFEATURES = "directfb x11"
I'm not sure which package you are adding that requires `libgtk2.0` in the first place? You need to experiment with your setup and unroll and understand if you really need gtk for the package you are trying to use and if there's a way to remove/simplify dependencies. Also, note that do we do not support `x11` with our offering.
Regards, Andreas