Hi,
We have the Zoom OMAP138 development kit from LogicPD, together with CCS 4.2.
I'm trying to setup the C6748 DSP to use the L2 RAM for the stack, but when configured this
way my program does not execute at all. I do not get any compiler or linker warnings, so I'm
not sure why it behaves in this manner. I have attached my declaration of the memory sections.
-stack 0x00010000
-heap 0x00008000
MEMORY
{
dsp_l2_ram: ORIGIN = 0x00800000 LENGTH = 0x00040000
shared_ram: ORIGIN = 0x80000000 LENGTH = 0x00020000
external_ram: ORIGIN = 0xC0000000 LENGTH = 0x08000000
arm_local_ram: ORIGIN = 0xFFFF0000 LENGTH = 0x00002000
}
SECTIONS
{
.text > dsp_l2_ram
.const > dsp_l2_ram
.bss > dsp_l2_ram
.far > dsp_l2_ram
.switch > dsp_l2_ram
.stack > dsp_l2_ram
.data > dsp_l2_ram
.cinit > dsp_l2_ram
.sysmem > dsp_l2_ram
.cio > dsp_l2_ram
}
Could someone please assist?
Regards
Reinier