This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28P65X: LAUNCHXL-F28P65X Flash Memory 32-bit Write

Part Number: LAUNCHXL-F28P65X
Other Parts Discussed in Thread: C2000WARE

Tool/software:

Hello,

I have an inquiry regarding Flash Memory Write.
I am currently using the LAUNCHXL-F28P65X board.

I am using the Flash example program provided in the C2000Ware_5_04_00_00 SDK. (C:\ti\c2000\C2000Ware_5_04_00_00\driverlib\f28p65x\examples\c28x\flash\CCS\f28p65x_eeprom_example.projectspec)

The example program writes 8 bytes to the flash memory at a time. I would like to write 4 bytes at a time, but when I try, an error occurs within the EEPROM_CheckStatus() function.

Is the minimum write size to the flash memory 8 bytes? I would like to know if there is a way to write 4 bytes at a time.

Below is the code of the example program.