This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Use String Descriptor with c5535 eZdsp



Hi,

I´m trying to enable the string descriptor in the audio framework demo that comes with the eZdsp to be able to give the device a product name in windows. In the demo code the string descriptor is not used.

I´m using the following descriptors:

const Uint16 stringLanId[STRING_LAN_ID_SZ] = 

    0x0000, 0x0304, 0x0409, 0x0000

};

const char *string_descriptor[STRING_DESCR_SZ] =

{

  " ",   /* This will eventually point to  the string descriptor */

  " man",           /* iManufacturer */

  " prod",                      /* iProductName */

  " ser",                       /* iSerial No :RomId - F# */

  " int",                     /* iInterface - Audio Class */

  NULL

};

These are then combined in AC_Open, where the stringLanId pointer is places first in the string descriptor.

I also change the device descriptor to use strings for iManufactutrer, iProduct and iSerialNumber, however this only results in "Code 10" that the USB-device could not start.

Are there more modifications of the demo code I have to do to make this work?

 

Thanks, Marcus