This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62: MCU MCAN0 and MCAN1 Configuration in Interrupt mode

Part Number: SK-AM62


Tool/software:

Hi Team,

I am configuring MCU MCAN0 and MCU MCAN1 in Interrupt mode.

In code I have enabled All interrupt. using IE register and Selected Interrupt line 1.

PFB image highlighted MCU domain CAN address are available to configure this register.

I have configured Interrupt for buffer 0

After adding request for transmission, I am reading below register to check Interrupts.

TC .i.e. Transmission bit is set when any CAN frame transmission completes

and DRX .i.e. Message stored in dedicated RX buffer is set when I receive any CAN frame.

Please confirm wheather my configuration is correct to configure MCAN in Interrupt mode.

PFB link of previous discussion

e2e.ti.com/.../sk-am62-how-to-use-a53-core-to-access-mcu-mcan0-and-mcu-mcan1-can-peripheral