This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4378: do_rootfs frailer "ti-sgx-ddk-um" after updating the meta-ti SDK to 9.2

Part Number: AM4378


Tool/software:

I am in the process of updating the yocto setup from dunfell to Kirkstone

In that process i upgraded the TI-SDK to 9.2 from 8.01 and poky 9.00 from 8.01. I am using the QT6.5 in my yocto setup

I upgraded my custom layer to Kirkstone layers

Once i am trying to create any image with"ti-sgx-ddk-km ti-sgx-ddk-um" added into the image i am getting below error, I am not sure what is the cause behind it and how to solve it.

ERROR: core-image-minimal-1.0-r0 do_rootfs: Postinstall scriptlets of ['ti-sgx-ddk-um'] have failed. If the intention is to defer them to first boot,
then please place them into pkg_postinst_ontarget:${PN} ().
Deferring to first boot via 'exit 1' is no longer supported.
Details of the failure are in /data/Bhavesh/fsp-release-9/build-lrd-am437x-lrd-5.10-rt-test/tmp/work/am437x_lrd-poky-linux-gnueabi/core-image-minimal/1.0-r0/temp/log.do_rootfs.
ERROR: Logfile of failure stored in: /data/platform/build-lrd-am437x-lrd-5.10-rt-test/tmp/work/am437x_lrd-poky-linux-gnueabi/core-image-minimal/1.0-r0/temp/log.do_rootfs.2356180
ERROR: Task (/data/platform/yocto/poky/meta/recipes-core/images/core-image-minimal.bb:do_rootfs) failed with exit code '1'

So far i know that PREFERRED_PROVIDER_virtual/gpudriver ?= "ti-sgx-ddk-km" is used in meta-ti/meta-ti-bsp/conf/machine/include/ti43x.inc and ti-sgx-ddk-km is depends on ti-sgx-ddk-um.

Even if I am creating core-image-minimal image and adding "ti-sgx-ddk-km ti-sgx-ddk-um" into the image i am getting same error

  • Once i am trying to create any image with"ti-sgx-ddk-km ti-sgx-ddk-um" add

    Since you mentioned that, we have just released AM437x SDK v9.3, see https://www.ti.com/tool/download/PROCESSOR-SDK-LINUX-AM437X. It has a MUCH improved/fixed graphics stack. I'd highly recommend you switch to this. If you still see build issues we need to compare the known-good SDK build/setup that you should be able to re-create, with your customized port.

    In that process i upgraded the TI-SDK to 9.2

    Don't use 9.2 tags for building for AM335x/AM437x. There was no SDK release for those devices made at this tag, hence no testing was done and the result is likely invalid.

    Regards, Andreas

  • Hi Andreas, Thank you so much for your reply. 

    I am also looking for using same yocto setup for AM437x and AM335x too, Also I am looking for the the AM62xx support too with the same yocto setup.

    I see as you suggested SDK v9.3 is also available for AM335x too which I can use. 

    No the question is, which latest single SDK version should I use that allows me to build image with Kirkstone yocto for AM335x and AM62xx boards.

  • No the question is, which latest single SDK version should I use that allows me to build image with Kirkstone yocto for AM335x and AM62xx boards

    I would not recommend using v9.x for AM6x devices. There have been many improvements since, some critical, such as MMC/SD driver routines, DM-firmware PLL routines, and many more. It would be quite difficult to identify all changes and backport them from SDK v10.1.

    Regards, Andreas

  • So to conclude it is suggested to use SDK v9.3 for am335x and am437x devices and for am62xx SDKv10.1 is suggested. Is this correct ?

    I tried the switching to SDK v9.3 in meta-ti with commit 963140e3b5820d6ebf54a4418946a628e0fea2c6 (HEAD, tag: cicd.kirkstone.202412041235, tag: 09.03.05) and recompile the image. still i am seeing the same error in there. 

    I am still looking for the way to compile an image on top of fresh SDK 9.3 and add "ti-sgx-ddk-km ti-sgx-ddk-um" packages into the image and check whether it complete the image build or not.

  • So to conclude it is suggested to use SDK v9.3 for am335x and am437x devices and for am62xx SDKv10.1 is suggested. Is this correct ?

    Correct.

    I am still looking for the way to compile an image on top of fresh SDK 9.3 and add "ti-sgx-ddk-km ti-sgx-ddk-um" packages into the image and check whether it complete the image build or not.

    I suggest re-creating the SDK build as it is intended, and then inspecting it to see what are significant differences vs. your setup. Often this is an exercise involving a lot of string searches (`grep`).

    Also have you looked at the detailed error log files referenced in the console build error message from your original post? It might be that the post-install script is not appropriate for your changed filesystem, so you might want to focus on that and see what needs to be tweaked there.

    Regards, Andreas

  • hi Andreas, As you suggested I crated the TI SDK build for 9.3.5 sdk, In that I tried adding ti-sgx-ddk-km and ti-sgx-ddk-um drivers. It gave the same error in there. After that once I investigated the older recipe of ti-sgx-ddk-um (TI-SDK 08.01.001) I observed that udev is used and if the yocto system is sysvinit then they are includeing update-rc.d class

    INITSCRIPT_NAME = "rc.pvr"
    INITSCRIPT_PARAMS = "defaults 8"
    
    PACKAGECONFIG ??= "udev"
    PACKAGECONFIG[udev] = "UDEV=true,,,udev"
    
    def use_sysvinit(d):
        return d.getVar('VIRTUAL-RUNTIME_init_manager') == 'sysvinit'
    
    inherit ${@oe.utils.ifelse(use_sysvinit(d), 'update-rc.d', '')}

    From the errors I was doubting about this error is something to do with the update-rc.d file and that is causing the error at rootfs time.

    If I update the PACKAGECONFIG = ""  then we are able to create the final image.

    I took the changes and added the into the yocto setup i am using to create my custom image. I am able to create the final image. But if i test the image i am not able to see any graphic on board. ( i am testing on am437x-sk board, in older image with older TI-SDK 8 and dunfell yocto I am using a qt based application which is showing a logo once the board is up) I am getting below errors

    Setting environment variables...Starting UI app... UI app started.
    root@Node:~# Detected locale "C" with character encoding "ANSI_X3.4-1968", which is not UTF-8.
    Qt depends on a UTF-8 locale, and has switched to "C.UTF-8" instead.
    If this causes problems, reconfigure your locale. See the locale(1) manual
    for more information.
    MESA: info: Loaded libpvr_dri_support.so
    PVR:(Error): PVRDRICreateScreenImpl: Failed to create display device (err=19) [0, ]
    MESA: info: Unloaded libpvr_dri_support.so
    MESA-LOADER: failed to open zink: /usr/lib/dri/zink_dri.so: cannot open shared object file: No such file or directory (search paths /usr/lib/dri, suffix _dri)
    failed to load driver: zink
    drmModeGetResources failed (Operation not supported)
    Cannot create window: no screens available
    

    My questions are

    1. What is the need of UDEV in ti-sgx-ddk-um driver. ( my understanding is it might me be needed to add the graphic driver into the kernel image)
    2. Is there any documentation i can refer to understand the updated ti sgx drivers.
    3. Right now to make the image work i have removed UDEV from PACKAGECONFIG variable. If it is required what should be the proper way to make it work
    4. Is there an yocto image/setup which i can use to take reference about how i can use graphics usign QT in updated TI SDK

    My end target to make the older QT application work with updated yocto and meta-ti sdk

    I am thinking that in the process of upgrading the yocto some of the points are missed from my end which could be causing this issue.

     

  • I'm currently on international business travel working at a customer site and not able to look into this further; will comment once I'm back in the office next week.

    Regards, Andreas

  • There has been no activity on this thread, so marking this closed as it might've been resolved offline