Hi there,
i am currently reading (and trying to understand) the sourcecode of the omx c6xtest example. is it correct that the vlpb component is running completely in the dsp (all the sourcecode under "ezsdk/component-sources/omx_05_02_00_15/packages/ti/omx/comp/vlpb/src")? - if not where is the cut between arm and dsp?
is it correct that this code of the vlpb component can be compiled also for the arm? because in the makefile the source files are included in the "SRCS_a8host" and the "SRCS_c6xdsp" variable. So if this is the case, the vlcp module can be started either on the dsp or the arm and supplies the functions over syslink?
If i want to implement an own omx module, which runs on the dsp, i just have to modify the vlpb module for my needs?
tia
Nico