Other Parts Discussed in Thread: OMAP-L138
Hi,
We are using a custom made board based on a OMAP-L138.
After upgrading Linux kernel to 3.1 from 2.6.37, We are getting problem while trying to use the DSPLink module.
0x8000800c (DSP_EMEMORY) seems to be the error-code, but it should be enough memory.
No changes in either DSPLink (except built for different kerneln versions) or the DSP-application is made. It still works perfect in 2.6.37.
I have tried to set "mem=xxxM" as bootargs to the kernel, but it does not help.
We are using DSPLink v1.65.00.03.
Any suggestions?
Thanks in advance
Debug output:
Entered PMGR_PROC_setup ()
toSetup : 1
Entered LDRV_moduleInit ()
linkCfg [0x5abc8]
Entered LDRV_getLinkCfg ()
linkCfg [0x5abc8]
knlLinkCfg [0xbf192308]
Entered LDRV_getLinkDspCfg ()
procId [0x0]
dspCfg [0x5b0bc]
knlLinkCfg [0xc8b8c000]
Leaving LDRV_getLinkDspCfg () status [0x8000]
Leaving LDRV_getLinkGppCfg () status [0x8000]
Entered LDRV_PROC_moduleInit ()
Leaving LDRV_PROC_moduleInit () status [0x8000]
Entered LDRV_SMM_moduleInit ()
Leaving LDRV_SMM_moduleInit () status [0x8000]
Entered LDRV_MPCS_moduleInit ()
Entered LDRV_MPCS_OS_moduleInit ()
Leaving LDRV_MPCS_OS_moduleInit () status [0x8000]
Leaving LDRV_MPCS_moduleInit () status [0x8000]
Entered LDRV_MPLIST_moduleInit ()
Leaving LDRV_MPLIST_moduleInit () status [0x8000]
Entered LDRV_RINGIO_moduleInit ()
Leaving LDRV_RINGIO_moduleInit () status [0x8000]
Leaving LDRV_moduleInit () status [0x8000]
Entered PMGR_MSGQ_setup ()
Entered LDRV_MSGQ_setup ()
Leaving LDRV_MSGQ_setup () status [0x8000]
Leaving PMGR_MSGQ_setup () status [0x8000]
Leaving PMGR_PROC_setup () status [0x8000]
Entered PMGR_PROC_attach ()
procId [0x0]
attr [0x0]
Entered LDRV_init ()
procId [0x0]
dspCfg [0x0]
Leaving LDRV_init () status [0x8000]
Entered LDRV_PROC_init ()
dspId [0x0]
DSP_init status [0x8000800c]
Entered LDRV_PROC_exit ()
dspId [0x0]
Assertion failed (dspState->halObject != NULL). File : /home/developer/projects/dsplink_linux_1_65_00_03/build/gpp/src/../../gpp/src/arch/DA8XXGEM/da8xxgem.c Line : 611
Leaving LDRV_PROC_exit () status [0x8000]
Leaving LDRV_PROC_init () status [0x8000800c]
Entered LDRV_exit ()
procId [0x0]
Leaving LDRV_exit () status [0x8000]
Leaving PMGR_PROC_attach () status [0x8000800c]
Entered PMGR_MSGQ_close ()
msgqQueue [0x10000]
Leaving PMGR_MSGQ_close () status [0x8000800b]
Entered PMGR_MSGQ_close ()
msgqQueue [0x10001]
Leaving PMGR_MSGQ_close () status [0x8000800b]
Entered PMGR_MSGQ_close ()
msgqQueue [0x10002]
Leaving PMGR_MSGQ_close () status [0x8000800b]
Entered PMGR_MSGQ_close ()
msgqQueue [0x10003]
Leaving PMGR_MSGQ_close () status [0x8000800b]
Entered PMGR_MSGQ_close ()
msgqQueue [0x10004]
Leaving PMGR_MSGQ_close () status [0x8000800b]
Entered PMGR_MSGQ_close ()
msgqQueue [0x10005]
Leaving PMGR_MSGQ_close () status [0x8000800b]
Entered PMGR_MSGQ_close ()
msgqQueue [0x10006]
Leaving PMGR_MSGQ_close () status [0x8000800b]
Entered PMGR_MSGQ_close ()
msgqQueue [0x10007]
Leaving PMGR_MSGQ_close () status [0x8000800b]
Entered PMGR_MSGQ_close ()
msgqQueue [0x10008]
Leaving PMGR_MSGQ_close () status [0x8000800b]
Entered PMGR_MSGQ_close ()
msgqQueue [0x10009]
Leaving PMGR_MSGQ_close () status [0x8000800b]
Entered PMGR_MSGQ_close ()
msgqQueue [0x1000a]
Leaving PMGR_MSGQ_close () status [0x8000800b]
Entered PMGR_MSGQ_close ()
msgqQueue [0x1000b]
Leaving PMGR_MSGQ_close () status [0x8000800b]
Entered PMGR_MSGQ_close ()
msgqQueue [0x1000c]
Leaving PMGR_MSGQ_close () status [0x8000800b]
Entered PMGR_MSGQ_close ()
msgqQueue [0x1000d]
Leaving PMGR_MSGQ_close () status [0x8000800b]
Entered PMGR_MSGQ_close ()
msgqQueue [0x1000e]
Leaving PMGR_MSGQ_close () status [0x8000800b]
Entered PMGR_MSGQ_close ()
msgqQueue [0x1000f]
Leaving PMGR_MSGQ_close () status [0x8000800b]
Entered PMGR_PROC_getSetupRefCount ()
PMGR_PROC_getSetupRefCount [1]
Leaving PMGR_PROC_getSetupRefCount ()
Entered PMGR_PROC_destroy ()
Entered PMGR_MSGQ_destroy ()
Entered LDRV_MSGQ_destroy ()
Leaving LDRV_MSGQ_destroy () status [0x8000]
Leaving PMGR_MSGQ_destroy () status [0x8000]
Entered LDRV_moduleExit ()
Entered LDRV_RINGIO_moduleExit ()
Leaving LDRV_RINGIO_moduleExit () status [0x8000]
Entered LDRV_MPLIST_moduleExit ()
Leaving LDRV_MPLIST_moduleExit () status [0x8000]
Entered LDRV_MPCS_moduleExit ()
Entered LDRV_MPCS_OS_moduleExit ()
Leaving LDRV_MPCS_OS_moduleExit () status [0x8000]
Leaving LDRV_MPCS_moduleExit () status [0x8000]
Entered LDRV_SMM_moduleExit ()
Leaving LDRV_SMM_moduleExit () status [0x8000]
Entered LDRV_PROC_moduleExit ()
Leaving LDRV_PROC_moduleExit () status [0x8000]
Entered LDRV_freeLinkDspCfg ()
procId [0x0]
knlLinkCfg [0xc8b8c000]
Leaving LDRV_freeLinkDspCfg () status [0x8000]
Entered LDRV_freeLinkGppCfg ()
knlLinkCfg [0xc8b8c000]
Leaving LDRV_freeLinkGppCfg () status [0x8000]
Leaving LDRV_moduleExit () status [0x8000]
Leaving PMGR_PROC_destroy () status [0x8008]