Tool/software:
Hi,
Were a using AM6442 in our custom board with linux sdk 10.01.10.04.
Our problem is related to the configuration of the ethernet ports. We use 1 cpsw port and 2 icssg port with MII. Two problems are encountered :
- We are unable to ping the cpsw port with static address or with a dhcp server. The interface is found but a ping from a pc does not work. When we change the transfer speed in the pc, the board detect that change.
- The other problem is with icssg who does not detect the phy: icssg-prueth icssg0-eth: couldn't connect to phy ethernet-phy@3. it's seems like the physic address in the device tree is not good but, i know for sure it's 3 because icssg port was detected with linux sdk 9.02.01.10. We started having this problem when we switch in linux sdk 10.01.10.04.
Here is the boot output and the device tree file
SPL initial stack usage: 13392 bytes
Trying to boot from MMC2
Authentication passed
Authentication passed
Loading Environment from nowhere... OK
Authentication passed
Authentication passed
Starting ATF on ARM64 core...
NOTICE: BL31: v2.11.0(release):v2.11.0-906-g58b25570c9-dirty
NOTICE: BL31: Built : 04:20:32, Nov 1 2024
I/TC:
I/TC: OP-TEE version: 4.4.0-dev (gcc version 13.3.0 (GCC)) #1 Fri Oct 18 17:45:2 7 UTC 2024 aarch64
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/ porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: GIC redistributor base address not provided
I/TC: Assuming default GIC group status and modifier
I/TC: SYSFW ABI: 4.0 (firmware rev 0x000a '10.1.8--v10.01.08 (Fiery Fox)')
I/TC: Activated SA2UL device
I/TC: Enabled firewalls for SA2UL TRNG device
I/TC: SA2UL TRNG initialized
I/TC: SA2UL Drivers initialized
I/TC: HUK Initialized
I/TC: Primary CPU switching to normal world boot
U-Boot SPL 2024.04-ti-g29d0c23d67ee (Nov 29 2024 - 11:41:54 +0000)
SYSFW ABI: 4.0 (firmware rev 0x000a '10.1.8--v10.01.08 (Fiery Fox)')
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed -1
Trying to boot from MMC2
Authentication passed
Authentication passed
U-Boot 2024.04-ti-g29d0c23d67ee (Nov 29 2024 - 11:41:54 +0000)
SoC: AM64X SR2.0 HS-FS
Model: Texas Instruments AM642 EVM
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed -1
DRAM: 2 GiB
Core: 98 devices, 31 uclasses, devicetree: separate
NAND: 0 MiB
MMC: mmc@fa10000: 0, mmc@fa00000: 1
Loading Environment from nowhere... OK
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed -1
Net: eth0: ethernet@8000000port@1
Warning: icssg1-eth-port@0 (eth2) using random MAC address - 3a:23:74:5f:a3:67
, eth2: icssg1-eth-port@0
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
574 bytes read in 40 ms (13.7 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
16894464 bytes read in 693 ms (23.2 MiB/s)
43748 bytes read in 43 ms (993.2 KiB/s)
Working FDT set to 88000000
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Working FDT set to 88000000
Loading Device Tree to 000000008fef2000, end 000000008fffffff ... OK
Working FDT set to 8fef2000
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 6.6.58-rt45-ti-rt-01780-gc79d7ef3a56f-dirty (oe-use r@oe-host) (aarch64-oe-linux-gcc (GCC) 13.3.0, GNU ld (GNU Binutils) 2.42.0.2024 0723) #1 SMP PREEMPT_RT Wed Nov 27 14:15:26 UTC 2024
[ 0.000000] Machine model: Texas Instruments AM642 EVM-Config Master board
[ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[ 0.000000] printk: legacy bootconsole [ns16550a0] enabled
[ 0.000000] efi: UEFI not found.
[ 0.000000] OF: reserved mem: 0x000000009e800000..0x000000009fffffff (24576 K iB) nomap non-reusable optee@9e800000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, s ize 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compa tible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a0000000..0x00000000a00fffff (1024 Ki B) nomap non-reusable r5f-dma-memory@a0000000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, s ize 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatibl e id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a0100000..0x00000000a0ffffff (15360 K iB) nomap non-reusable r5f-memory@a0100000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, s ize 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compa tible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a1000000..0x00000000a10fffff (1024 Ki B) nomap non-reusable r5f-dma-memory@a1000000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, s ize 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatibl e id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a1100000..0x00000000a1ffffff (15360 K iB) nomap non-reusable r5f-memory@a1100000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, s ize 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a2000000, compa tible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a2000000..0x00000000a20fffff (1024 Ki B) nomap non-reusable r5f-dma-memory@a2000000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, s ize 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a2100000, compatibl e id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a2100000..0x00000000a2ffffff (15360 K iB) nomap non-reusable r5f-memory@a2100000
teI / TC0.:0 0S0e0co00n]d aRreys eCrPUv e1d mienimotriayl: izcrienag
d IDM/AT Cm:e mSoercoyn pdoaoryl aCtPU 0x10 0s0w0it0c0h00ian3g0 t00o0 0no0r, o asil zew o1r lMdi Bb
ot[
0.000000] OF: reserved mem: initialized node r5f-dma-memory@a3000000, compat ible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a3000000..0x00000000a30fffff (1024 Ki B) nomap non-reusable r5f-dma-memory@a3000000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a3100000, s ize 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a3100000, compatibl e id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a3100000..0x00000000a3ffffff (15360 K iB) nomap non-reusable r5f-memory@a3100000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, s ize 1 MiB
[ 0.000000] OF: reserved mem: initialized node m4f-dma-memory@a4000000, compa tible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a4000000..0x00000000a40fffff (1024 Ki B) nomap non-reusable m4f-dma-memory@a4000000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, s ize 15 MiB
[ 0.000000] OF: reserved mem: initialized node m4f-memory@a4100000, compatibl e id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a4100000..0x00000000a4ffffff (15360 K iB) nomap non-reusable m4f-memory@a4100000
[ 0.000000] OF: reserved mem: 0x00000000a5000000..0x00000000a57fffff (8192 Ki B) nomap non-reusable ipc-memories@a5000000
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x000000009e7fffff]
[ 0.000000] node 0: [mem 0x000000009e800000-0x00000000a57fffff]
[ 0.000000] node 0: [mem 0x00000000a5800000-0x00000000ffffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] cma: Reserved 32 MiB at 0x00000000fbe00000 on node -1
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.5
[ 0.000000] percpu: Embedded 21 pages/cpu s46656 r8192 d31168 u86016
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: kernel page table isolation disabled by kernel conf iguration
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] alternatives: applying boot alternatives
[ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmi o32,0x02800000 omap2-nand.0:2m(NAND.tiboot3),2m(NAND.tispl),2m(NAND.tiboot3.back up),4m(NAND.u-boot),256k(NAND.u-boot-env),256k(NAND.u-boot-env.backup),-(NAND.fi le-system) root=PARTUUID=076c4a2a-02 rw rootfstype=ext4 rootwait
[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 516096
[ 0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[ 0.000000] software IO TLB: area num 2.
[ 0.000000] software IO TLB: mapped [mem 0x00000000f7c00000-0x00000000fbc0000 0] (64MB)
[ 0.000000] Memory: 1830036K/2097152K available (10496K kernel code, 1202K rw data, 2512K rodata, 2176K init, 457K bss, 234348K reserved, 32768K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[ 0.000000] rcu: RCU_SOFTIRQ processing moved to rcuc kthreads.
[ 0.000000] No expedited grace period (rcu_normal_after_boot).
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 100 ji ffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 256 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] Root IRQ handler: 0xffff8000800100c0
[ 0.000000] GICv3: GICv3 features: 16 PPIs
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001840000
[ 0.000000] ITS [mem 0x01820000-0x0182ffff]
[ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->1 9
[ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80800000 (flat, esz 8, psz 64K, shr 0)
[ 0.000000] ITS: using cache flushing for cmd queue
[ 0.000000] GICv3: using LPI property table @0x0000000080030000
[ 0.000000] GIC: using cache flushing for LPI property table
[ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x000000008004000 0
[ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles : 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[ 0.000001] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 43980 46511102ns
[ 0.000236] Console: colour dummy device 80x25
[ 0.000300] Calibrating delay loop (skipped), value calculated using timer fr equency.. 400.00 BogoMIPS (lpj=200000)
[ 0.000313] pid_max: default: 32768 minimum: 301
[ 0.000395] LSM: initializing lsm=capability,selinux,integrity
[ 0.000420] SELinux: Initializing.
[ 0.000620] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, line ar)
[ 0.000645] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.009103] rcu: Hierarchical SRCU implementation.
[ 0.009116] rcu: Max phase no-delay instances is 400.
[ 0.051411] Platform MSI: msi-controller@1820000 domain created
[ 0.051666] PCI/MSI: /bus@f4000/interrupt-controller@1800000/msi-controller@1 820000 domain created
[ 0.051760] EFI services will not be available.
[ 0.108542] smp: Bringing up secondary CPUs ...
[ 0.250952] Detected VIPT I-cache on CPU1
[ 0.251061] GICv3: CPU1: found redistributor 1 region 0:0x0000000001860000
[ 0.251078] GICv3: CPU1: using allocated LPI pending table @0x000000008005000 0
[ 0.251139] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.299575] smp: Brought up 1 node, 2 CPUs
[ 0.299584] SMP: Total of 2 processors activated.
[ 0.299590] CPU features: detected: 32-bit EL0 Support
[ 0.299594] CPU features: detected: CRC32 instructions
[ 0.299649] CPU: All CPU(s) started at EL2
[ 0.299652] alternatives: applying system-wide alternatives
[ 0.302588] devtmpfs: initialized
[ 0.314511] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, ma x_idle_ns: 1911260446275000 ns
[ 0.314542] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[ 0.316087] pinctrl core: initialized pinctrl subsystem
[ 0.316811] DMI not present or invalid.
[ 0.317400] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.319428] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[ 0.319754] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allo cations
[ 0.319970] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic al locations
[ 0.320062] audit: initializing netlink subsys (disabled)
[ 0.320662] audit: type=2000 audit(0.319:1): state=initialized audit_enabled= 0 res=1
[ 0.321119] thermal_sys: Registered thermal governor 'step_wise'
[ 0.321411] ASID allocator initialised with 65536 entries
[ 0.327011] /bus@f4000/interrupt-controller@1800000: Fixed dependency cycle(s ) with /bus@f4000/interrupt-controller@1800000
[ 0.337217] Modules: 28512 pages in range for non-PLT usage
[ 0.337232] Modules: 520032 pages in range for PLT usage
[ 0.338165] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.338182] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[ 0.338188] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.338192] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[ 0.338197] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.338201] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[ 0.338206] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.338210] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[ 1.027214] k3-chipinfo 43000014.chipid: Family:AM64X rev:SR2.0 JTAGID[0x1bb3 802f] Detected
[ 1.028069] iommu: Default domain type: Translated
[ 1.028082] iommu: DMA domain TLB invalidation policy: strict mode
[ 1.028572] SCSI subsystem initialized
[ 1.029014] usbcore: registered new interface driver usbfs
[ 1.029055] usbcore: registered new interface driver hub
[ 1.029097] usbcore: registered new device driver usb
[ 1.029747] pps_core: LinuxPPS API ver. 1 registered
[ 1.029755] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giome tti <giometti@linux.it>
[ 1.029775] PTP clock support registered
[ 1.030050] EDAC MC: Ver: 3.0.0
[ 1.030564] scmi_core: SCMI protocol bus registered
[ 1.030935] FPGA manager framework
[ 1.031079] Advanced Linux Sound Architecture Driver Initialized.
[ 1.032671] clocksource: Switched to clocksource arch_sys_counter
[ 1.032939] VFS: Disk quotas dquot_6.6.0
[ 1.032974] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 1.042389] NET: Registered PF_INET protocol family
[ 1.042762] IP idents hash table entries: 32768 (order: 6, 262144 bytes, line ar)
[ 1.044972] tcp_listen_portaddr_hash hash table entries: 1024 (order: 3, 4096 C bytes, linearI/)T
b:[ R e se1.r0v4e5d 03sh0a] rTead bmlee-mpoerryt uirsb ehnaasblh etda
sleI /enTtCr: ieDysn: a6mi55c3 6s h(aorredde rm:e m6o,r y2 6i2s1 e4n4 abbyltede
or lI/inTeCa:r )N
m[a l W1or.l0d4 5v04i2rt]u TalCiP zaesttiaobnl sisuhpepdor hta sihs tdaibs rabel eendt
ieIs/T:C 1:6 A3s8y4n (cohrrdoenrou: s5 ,no 1t3i1fi0c72a tiboytnse s,a rlei ndei lsarb)
ed[
1.045275] TCP bind hash table entries: 16384 (order: 8, 1310720 bytes, linear )
[ 1.046880] TCP: Hash tables configured (established 16384 bind 16384)
[ 1.047134] UDP hash table entries: 1024 (order: 4, 98304 bytes, linear)
[ 1.047288] UDP-Lite hash table entries: 1024 (order: 4, 98304 bytes, linear)
[ 1.047634] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 1.048300] RPC: Registered named UNIX socket transport module.
[ 1.048309] RPC: Registered udp transport module.
[ 1.048313] RPC: Registered tcp transport module.
[ 1.048316] RPC: Registered tcp-with-tls transport module.
[ 1.048319] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 1.048335] PCI: CLS 0 bytes, default 64
[ 1.049915] Initialise system trusted keyrings
[ 1.050182] workingset: timestamp_bits=62 max_order=19 bucket_order=0
[ 1.050561] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 1.050933] NFS: Registering the id_resolver key type
[ 1.050977] Key type id_resolver registered
[ 1.050981] Key type id_legacy registered
[ 1.051004] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 1.051011] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering ...
[ 1.089587] Key type asymmetric registered
[ 1.089605] Asymmetric key parser 'x509' registered
[ 1.089722] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 2 44)
[ 1.089730] io scheduler mq-deadline registered
[ 1.089736] io scheduler kyber registered
[ 1.089776] io scheduler bfq registered
[ 1.095271] pinctrl-single 4084000.pinctrl: 33 pins, size 132
[ 1.095911] pinctrl-single f4000.pinctrl: 180 pins, size 720
[ 1.097654] pinctrl-single a40000.pinctrl: 512 pins, size 2048
[ 1.106476] Serial: 8250/16550 driver, 12 ports, IRQ sharing enabled
[ 1.122426] loop: module loaded
[ 1.123910] megasas: 07.725.01.00-rc1
[ 1.129311] tun: Universal TUN/TAP device driver, 1.6
[ 1.130728] VFIO - User Level meta-driver version: 0.3
[ 1.132053] usbcore: registered new interface driver usb-storage
[ 1.137875] i2c_dev: i2c /dev entries driver
[ 1.138765] sdhci: Secure Digital Host Controller Interface driver
[ 1.138777] sdhci: Copyright(c) Pierre Ossman
[ 1.139015] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.140015] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 1.141059] usbcore: registered new interface driver usbhid
[ 1.141069] usbhid: USB HID core driver
[ 1.142216] optee: probing for conduit method.
[ 1.142254] optee: revision 4.4 (8f645256efc0dc66)
[ 1.175359] optee: dynamic shared memory is enabled
[ 1.176365] random: crng init done
[ 1.176807] optee: initialized driver
[ 1.179539] Initializing XFRM netlink socket
[ 1.179590] NET: Registered PF_PACKET protocol family
[ 1.179759] Key type dns_resolver registered
[ 1.192766] Loading compiled-in X.509 certificates
[ 1.208149] ti-sci 44043000.system-controller: ABI: 4.0 (firmware rev 0x000a '10.1.8--v10.01.08 (Fiery Fox)')
[ 1.368358] omap_i2c 20000000.i2c: bus 0 rev0.12 at 400 kHz
[ 1.368789] ti-sci-intr 4210000.interrupt-controller: Interrupt Router 5 doma in created
[ 1.369014] ti-sci-intr bus@f4000:interrupt-controller@a00000: Interrupt Rout er 3 domain created
[ 1.369385] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator d omain 28 created
[ 1.373095] ti-udma 485c0100.dma-controller: Number of rings: 68
[ 1.375410] ti-udma 485c0100.dma-controller: Channels: 24 (bchan: 12, tchan: 6, rchan: 6)
[ 1.377993] ti-udma 485c0000.dma-controller: Number of rings: 288
[ 1.393021] ti-udma 485c0000.dma-controller: Channels: 44 (tchan: 29, rchan: 15)
[ 1.398158] printk: console [ttyS2] disabled
[ 1.514356] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 312, base_baud = 3 000000) is a 8250
[ 1.523255] printk: console [ttyS2] enabled
[ 1.523263] printk: legacy bootconsole [ns16550a0] disabled
[ 1.526829] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode
[ 1.560691] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 10 00000
[ 1.563289] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver Micrel KSZ9031 Gigabit PHY
[ 1.563356] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss vers ion 0x6BA00903, cpsw version 0x6BA80903 Ports: 3 quirks:00000006
[ 1.563543] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.4
[ 1.563550] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512
[ 1.564454] pps pps0: new PPS source ptp0
[ 1.564908] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000 000, add_val:1 pps:1
[ 1.624865] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 16
[ 1.631610] am65-cpts 39000000.cpts: CPTS ver 0x4e8a010c, freq:500000000, add _val:1 pps:0
[ 1.634134] mmc0: CQHCI version 5.10
[ 1.636459] mmc1: CQHCI version 5.10
[ 1.651701] cdns-torrent-phy f000000.serdes: No available link subnodes found
[ 1.651759] cdns-torrent-phy: probe of f000000.serdes failed with error -22
[ 1.657286] clk: Disabling unused clocks
[ 1.680884] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64 -bit
[ 1.680926] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64 -bit
[ 1.686041] ALSA device list:
[ 1.686056] No soundcards found.
[ 1.702472] Waiting for root device PARTUUID=076c4a2a-02...
[ 1.715537] mmc1: new high speed SDXC card at address 5048
[ 1.716456] mmcblk1: mmc1:5048 SD128 119 GiB
[ 1.719765] mmcblk1: p1 p2
[ 1.790103] mmc0: Command Queue Engine enabled
[ 1.790183] mmc0: new HS200 MMC card at address 0001
[ 1.791083] mmcblk0: mmc0:0001 G1M15L 29.6 GiB
[ 1.793394] mmcblk0boot0: mmc0:0001 G1M15L 31.5 MiB
[ 1.795194] mmcblk0boot1: mmc0:0001 G1M15L 31.5 MiB
[ 1.796808] mmcblk0rpmb: mmc0:0001 G1M15L 4.00 MiB, chardev (239:0)
[ 2.024495] EXT4-fs (mmcblk1p2): recovery complete
[ 2.026940] EXT4-fs (mmcblk1p2): mounted filesystem eaef9f1f-ba30-47a0-bea2-f 4db1f31bcd4 r/w with ordered data mode. Quota mode: none.
[ 2.027061] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 2.027855] devtmpfs: mounted
[ 2.029395] Freeing unused kernel memory: 2176K
[ 2.029527] Run /sbin/init as init process
[ 2.568375] systemd[1]: System time before build time, advancing clock.
[ 2.658064] NET: Registered PF_INET6 protocol family
[ 2.659449] Segment Routing with IPv6
[ 2.659484] In-situ OAM (IOAM) with IPv6
[ 2.702385] systemd[1]: systemd 255.13^ running in system mode (+PAM -AUDIT - SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CUR L -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUA LITY -P11KIT -QRENCODE -TPM2 -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK -XKBCOMM ON +UTMP +SYSVINIT default-hierarchy=unified)
[ 2.702483] systemd[1]: Detected architecture arm64.
Welcome to Arago 2023.10!
[ 2.747060] systemd[1]: Hostname set to <am64xx-evm>.
[ 3.286984] systemd[1]: /usr/lib/systemd/system/bt-enable.service:9: Standard output type syslog is obsolete, automatically updating to journal. Please updat e your unit file, and consider removing the setting altogether.
[ 3.442378] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
[ 3.541168] systemd[1]: Queued start job for default target Graphical Interfa ce.
[ 3.569135] systemd[1]: Created slice Slice /system/getty.
[ OK ] Created slice Slice /system/getty.
[ 3.584840] systemd[1]: Created slice Slice /system/modprobe.
[ OK ] Created slice Slice /system/modprobe.
[ 3.600791] systemd[1]: Created slice Slice /system/serial-getty.
[ OK ] Created slice Slice /system/serial-getty.
[ 3.617020] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 3.631399] systemd[1]: Started Dispatch Password Requests to Console Directo ry Watch.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ 3.651387] systemd[1]: Started Forward Password Requests to Wall Directory W atch.
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ 3.668109] systemd[1]: Expecting device /dev/ttyS2...
Expecting device /dev/ttyS2...
[ 3.681148] systemd[1]: Reached target Path Units.
[ OK ] Reached target Path Units.
[ 3.692027] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 3.706018] systemd[1]: Reached target Slice Units.
[ OK ] Reached target Slice Units.
[ 3.717049] systemd[1]: Reached target Swaps.
[ OK ] Reached target Swaps.
[ 3.730526] systemd[1]: Listening on RPCbind Server Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ 3.746073] systemd[1]: Reached target RPC Port Mapper.
[ OK ] Reached target RPC Port Mapper.
[ 3.772395] systemd[1]: Listening on Process Core Dump Socket.
[ OK ] Listening on Process Core Dump Socket.
[ 3.787539] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 3.804705] systemd[1]: Listening on Journal Audit Socket.
[ OK ] Listening on Journal Audit Socket.
[ 3.820075] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 3.836202] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 3.851272] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 3.875108] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 3.889953] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 3.905109] systemd[1]: Listening on User Database Manager Socket.
[ OK ] Listening on User Database Manager Socket.
[ 3.931159] systemd[1]: Mounting Huge Pages File System...
Mounting Huge Pages File System...
[ 3.956264] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 3.981281] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 3.996599] systemd[1]: Kernel Trace File System was skipped because of an un met condition check (ConditionPathExists=/sys/kernel/tracing).
[ 4.013301] systemd[1]: Mounting Temporary Directory /tmp...
Mounting Temporary Directory /tmp...
[ 4.043080] systemd[1]: Starting Create List of Static Device Nodes...
Starting Create List of Static Device Nodes...
[ 4.061597] systemd[1]: Starting Load Kernel Module configfs...
Starting Load Kernel Module configfs...
[ 4.094916] systemd[1]: Starting Load Kernel Module drm...
Starting Load Kernel Module drm...
[ 4.128725] systemd[1]: Starting Load Kernel Module fuse...
Starting Load Kernel Module fuse...
[ 4.164651] systemd[1]: Starting RPC Bind...
Starting RPC Bind...
[ 4.177467] systemd[1]: File System Check on Root Device was skipped because of an unmet condition check (ConditionPathIsReadWrite=!/).
[ 4.182758] systemd[1]: systemd-journald.service: unit configures an IP firew all, but the local system does not support BPF/cgroup firewalling.
[ 4.182832] systemd[1]: systemd-journald.service: (This warning is only shown for the first unit using IP firewalling.)
[ 4.216546] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 4.244785] fuse: init (API version 7.39)
[ 4.257573] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 4.287585] systemd[1]: Starting Generate network units from Kernel command l ine...
Starting Generate network units from Kernel command line...
[ 4.322595] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 4.337558] systemd-journald[115]: Collecting audit messages is enabled.
[ 4.372639] systemd[1]: Starting Coldplug All udev Devices...
Starting Coldplug All udev Devices...
[ 4.431762] systemd[1]: Started RPC Bind.
[ 4.435887] cryptodev: loading out-of-tree module taints kernel.
[ OK ] Started RPC Bind.
[ 4.446201] cryptodev: driver 1.14 loaded.
[ 4.462908] systemd[1]: Mounted Huge Pages File System.
[ OK ] Mounted Huge Pages File System.
[ 4.490815] systemd[1]: Mounted POSIX Message Queue File System.
[ OK ] Mounted POSIX Message Queue File System.
[ 4.514386] systemd[1]: Started Journal Service.
[ 4.522756] EXT4-fs (mmcblk1p2): re-mounted eaef9f1f-ba30-47a0-bea2-f4db1f31b cd4 r/w. Quota mode: none.
[ OK ] Started Journal Service.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted Temporary Directory /tmp.
[ OK ] Finished Create List of Static Device Nodes.
[ OK ] Finished Load Kernel Module configfs.
[ OK ] Finished Load Kernel Module drm.
[ OK ] Finished Load Kernel Module fuse.
[ OK ] Finished Load Kernel Modules.
[ OK ] Finished Generate network units from Kernel command line.
[ OK ] Finished Remount Root and Kernel File Systems.
Mounting FUSE Control File System...
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
Starting Apply Kernel Variables...
Starting Create Static Device Nodes in /dev gracefully...
[ OK ] Mounted FUSE Control File System.
[ OK ] Mounted Kernel Configuration File System.
[ 4.917224] systemd-journald[115]: Received client request to flush runtime j ournal.
[ OK ] Finished Flush Journal to Persistent Storage.
[ OK ] Finished Apply Kernel Variables.
[ OK ] Finished Create Static Device Nodes in /dev gracefully.
Starting Create Static Device Nodes in /dev...
[ OK ] Finished Create Static Device Nodes in /dev.
[ OK ] Reached target Preparation for Local File Systems.
Mounting /var/volatile...
Starting Rule-based Manager for Device Events and Files...
[ OK ] Mounted /var/volatile.
Starting Load/Save OS Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create System Files and Directories...
[ OK ] Finished Load/Save OS Random Seed.
Starting User Database Manager...
[ OK ] Finished Create System Files and Directories.
Starting Network Name Resolution...
Starting Network Time Synchronization...
Starting Record System Boot/Shutdown in UTMP...
[ OK ] Finished Coldplug All udev Devices.
[ OK ] Finished Record System Boot/Shutdown in UTMP.
[ OK ] Started User Database Manager.
[ OK ] Started Rule-based Manager for Device Events and Files.
[ OK ] Found device /dev/ttyS2.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Time Set.
[ OK ] Started Network Name Resolution.
[ OK ] Reached target Host and Network Name Lookups.
[ OK ] Reached target System Initialization.
[ OK ] Started Daily rotation of log files.
[ OK ] Started Timer service to update the IP on OLED each 10s.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timer Units.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
Starting Docker Socket for the API...
[ OK ] Listening on dropbear.socket.
[ OK ] Listening on PC/SC Smart Card Daemon Activation Socket.
Starting D-Bus System Message Bus...
Starting Reboot and dump vmcore via kexec...
[ OK ] Listening on Docker Socket for the API.
[ OK ] Finished Reboot and dump vmcore via kexec.
[ OK ] Started D-Bus System Message Bus.
[ 7.940506] dbus-broker-lau[257]: memfd_create() called without MFD_EXEC or M FD_NOEXEC_SEAL set
[ OK ] Reached target Socket Units.
[ OK ] Reached target Basic System.
[ OK ] Started Job spooling tools.
Starting Avahi mDNS/DNS-SD Stack...
[ OK ] Started Periodic Command Scheduler.
[ 8.361422] omap-mailbox 29020000.mailbox: omap mailbox rev 0x66fc9100
[ 8.376910] omap-mailbox 29040000.mailbox: omap mailbox rev 0x66fc9100
[ 8.384291] omap-mailbox 29060000.mailbox: omap mailbox rev 0x66fc9100
Starting Print notice about GPLv3 packages...
[ 8.404059] rtc-rv3028 0-0052: registered as rtc0
[ 8.409433] rtc-rv3028 0-0052: setting system clock to 2024-12-23T23:20:37 UT C (1734996037)
Starting IPv6 Packet Filtering Framework...
Starting IPv4 Packet Filtering Framework...
[ OK ] Started irqbalance daemon.
Starting Telephony service...
[ 8.767702] platform 78000000.r5f: configured R5F for remoteproc mode
[ 8.768477] platform 78000000.r5f: assigned reserved memory node r5f-dma-memo ry@a0000000
[ 8.769170] remoteproc remoteproc0: 78000000.r5f is available
[ 8.820873] remoteproc remoteproc0: powering up 78000000.r5f
[ 8.820975] remoteproc remoteproc0: Booting fw image am64-main-r5f0_0-fw, siz e 86352
[ 8.834133] rproc-virtio rproc-virtio.0.auto: assigned reserved memory node r 5f-dma-memory@a0000000
[ 8.838593] platform 78200000.r5f: configured R5F for remoteproc mode
[ 8.839866] platform 78200000.r5f: assigned reserved memory node r5f-dma-memo ry@a1000000
[ 8.895016] remoteproc remoteproc1: 78200000.r5f is available
[ 8.906391] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 8.906543] rproc-virtio rproc-virtio.0.auto: registered virtio0 (type 7)
[ 8.906555] remoteproc remoteproc0: remote processor 78000000.r5f is now up
[ 8.907297] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe
[ 8.920068] remoteproc remoteproc1: powering up 78200000.r5f
[ 8.920105] remoteproc remoteproc1: Booting fw image am64-main-r5f0_1-fw, siz e 141772
[ 8.927883] rproc-virtio rproc-virtio.1.auto: assigned reserved memory node r 5f-dma-memory@a1000000
[ 8.938894] virtio_rpmsg_bus virtio1: rpmsg host is online
[ 8.938952] rproc-virtio rproc-virtio.1.auto: registered virtio1 (type 7)
[ 8.938963] remoteproc remoteproc1: remote processor 78200000.r5f is now up
[ 8.939582] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xe
[ 8.978339] platform 78400000.r5f: configured R5F for remoteproc mode
[ 8.980877] platform 78400000.r5f: assigned reserved memory node r5f-dma-memo ry@a2000000
[ 8.988539] remoteproc remoteproc2: 78400000.r5f is available
Starting Expand the rootfs partiti…to full s[ 9.016841] remoteproc r emoteproc2: powering up 78400000.r5f
ize of the boot device....
[ 9.016931] remoteproc remoteproc2: Booting fw image am64-main-r5f1_0-fw, siz e 93260
[ 9.026768] rproc-virtio rproc-virtio.2.auto: assigned reserved memory node r 5f-dma-memory@a2000000
[ 9.032101] virtio_rpmsg_bus virtio2: rpmsg host is online
[ 9.032191] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0xe
[ 9.032230] rproc-virtio rproc-virtio.2.auto: registered virtio2 (type 7)
[ 9.032242] remoteproc remoteproc2: remote processor 78400000.r5f is now up
[ 9.032791] platform 78600000.r5f: configured R5F for remoteproc mode
[ 9.034048] platform 78600000.r5f: assigned reserved memory node r5f-dma-memo ry@a3000000
[ 9.035781] remoteproc remoteproc3: 78600000.r5f is available
[ 9.060567] remoteproc remoteproc3: powering up 78600000.r5f
[ 9.060604] remoteproc remoteproc3: Booting fw image am64-main-r5f1_1-fw, siz e 91520
[ 9.073520] rproc-virtio rproc-virtio.3.auto: assigned reserved memory node r 5f-dma-memory@a3000000
[ 9.082330] virtio_rpmsg_bus virtio3: rpmsg host is online
[ 9.082423] rproc-virtio rproc-virtio.3.auto: registered virtio3 (type 7)
[ 9.082434] remoteproc remoteproc3: remote processor 78600000.r5f is now up
[ 9.083361] virtio_rpmsg_bus virtio3: creating channel rpmsg_chrdev addr 0xe
Starting User Login Management...
Starting Telnet Server...
[ OK ] Finished IPv6 Packet Filtering Framework.
[ OK ] Finished IPv4 Packet Filtering Framework.
[ OK ] Finished Telnet Server.
[ OK ] Started Telephony service.
[ OK ] Reached target Preparation for Network.
Starting Network Configuration...
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ 9.659837] remoteproc remoteproc4: 3000a000.txpru is available
[ 9.665801] remoteproc remoteproc5: 3000c000.txpru is available
[ 9.674773] remoteproc remoteproc6: 3008a000.txpru is available
[ 9.681215] remoteproc remoteproc7: 3008c000.txpru is available
[ 9.974315] Bluetooth: Core ver 2.22
[ 9.979171] NET: Registered PF_BLUETOOTH protocol family
[ 9.979189] Bluetooth: HCI device and connection manager initialized
[ 9.979216] Bluetooth: HCI socket layer initialized
[ 9.979230] Bluetooth: L2CAP socket layer initialized
[ 9.979264] Bluetooth: SCO socket layer initialized
[ OK ] Finished Expand the rootfs partition to full size of the boot device..
[ OK ] Created slice Slice /system/tee-supplicant.
[ OK ] Started TEE Supplicant on teepriv0.
[ OK ] Started User Login Management.
[ 10.319859] remoteproc remoteproc8: 30006000.rtu is available
[ 10.337307] remoteproc remoteproc9: 30034000.pru is available
[ 10.523245] remoteproc remoteproc10: 30004000.rtu is available
[ 10.533438] cfg80211: Loading compiled-in X.509 certificates for regulatory d atabase
[ 10.542341] remoteproc remoteproc11: 300b4000.pru is available
[ 10.560454] remoteproc remoteproc12: 30084000.rtu is available
[ 10.573412] remoteproc remoteproc13: 30038000.pru is available
[ 10.604516] remoteproc remoteproc14: 300b8000.pru is available
[ 10.615498] remoteproc remoteproc15: 30086000.rtu is available
[ 10.620853] Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 10.639852] Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600 '
[ 10.643090] icssg-prueth icssg0-eth: port 1: using random MAC addr: 0e:f4:39: d9:60:f7
[ 10.703312] icssg-prueth icssg0-eth: couldn't connect to phy ethernet-phy@3
[ 10.703389] icssg-prueth icssg0-eth: can't connect to MII0 PHY, error --19
[ OK ] Started Network Configuration.
[ 11.180748] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] drive r [Micrel KSZ9031 Gigabit PHY] (irq=POLL)
[ 11.181845] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii l ink mode
[ OK ] Finished Virtual Console Setup.
[ OK ] Created slice Slice /system/systemd-fsck.
Expecting device /dev/mmcblk1p1...
[ OK ] Reached target Network.
[ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
Starting Enable and configure wl18xx bluetooth stack...
Starting containerd container runtime...
Starting LLDP daemon...
[ OK ] Started Netperf Benchmark Server.
Starting Simple Network Management Protocol (SNMP) Daemon....
Starting Wait for Network to be Configured...
Starting Permit User Sessions...
[ OK ] Finished Enable and configure wl18xx bluetooth stack.
[ OK ] Finished Permit User Sessions.
[ OK ] Found device /dev/mmcblk1p1.
[ OK ] Started LLDP daemon.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS2.
[ OK ] Reached target Login Prompts.
Starting Synchronize System and HW clocks...
Starting File System Check on /dev/mmcblk1p1...
[ OK ] Finished Synchronize System and HW clocks.
[ OK ] Finished File System Check on /dev/mmcblk1p1.
Mounting /run/media/boot-mmcblk1p1...
[ OK ] Mounted /run/media/boot-mmcblk1p1.
[ OK ] Started Simple Network Management Protocol (SNMP) Daemon..
[ 14.308646] am65-cpsw-nuss 8000000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ OK ] Started containerd container runtime.
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPL-3.0 packages:
adwaita-icon-theme-symbolic
autoconf
bash-dev
bash
bc
binutils
cifs-utils
coreutils-stdbuf
coreutils
cpio
cpp-symlinks
cpp
dosfstools
elfutils-dev
elfutils
findutils
g++-symlinks
g++
gawk
gcc-symlinks
gcc
gdb
gdbserver
gettext
glmark2
gnu-config
grub-common
grub-editenv
grub-efi
gzip
hidapi
kbd-dev
kbd-keymaps-pine
less
libasm1
libatomic-dev
libatomic1
libbfd
libdebuginfod1
libdw1
libelf1
libgcc-s-dev
libgcc1
libgdbm-compat4
libgdbm-dev
libgdbm6
libgettextlib
libgettextsrc
libgmp-dev
libgmp10
libgmpxx4
libgnutls-dev
libgnutls-openssl27
libidn2-0
libidn2-dev
libmpc3
libmpfr6
libopcodes
libqt5charts-examples
libqt5charts-plugins
libqt5charts-qmlplugins
libqt5charts5
libqt5serialport-examples
libqt5serialport-plugins
libqt5serialport-qmlplugins
libqt5serialport5
libqt5svg-examples
libqt5svg-plugins
libqt5svg-qmlplugins
libqt5svg5
libqt5virtualkeyboard-plugins
libqt5virtualkeyboard-qmlplugins
libqt5virtualkeyboard5
libreadline-dev
libreadline8
libstdc++-dev
libstdc++6
libtasn1-dev
libunistring-dev
libunistring5
m4
make
nettle-dev
nettle
parted
piglit
qt3d-plugins
qt3d-qmlplugins
qt3d
qtbase-examples
qtbase-plugins
qtbase-qmlplugins
qtbase
qtconnectivity-plugins
qtconnectivity-qmlplugins
qtconnectivity
qtdeclarative-plugins
qtdeclarative-qmlplugins
qtdeclarative-tools
qtdeclarative
qtgraphicaleffects-qmlplugins
qtlocation-examples
qtlocation-plugins
qtlocation-qmlplugins
qtlocation
qtmultimedia-examples
qtmultimedia-plugins
qtmultimedia-qmlplugins
qtmultimedia
qtquics-qmlplugins.control
qtquics2-plugins.control
qtquics2-qmlplugins.control
qtquics2.control
qtscript-examples
qtscript-plugins
qtscript-qmlplugins
qtscript
qtwayland-examples
qtwayland-plugins
qtwayland-qmlplugins
qtwayland
tar
which
If you do not wish to distribute GPL-3.0 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project am64xx-evm ttyS2
Arago 2023.10 am64xx-evm ttyS2
am64xx-evm login: root
[ 21.765512] audit: type=1006 audit(1734996050.855:2): pid=874 uid=0 subj=kern el old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1
[ 21.765777] audit: type=1300 audit(1734996050.855:2): arch=c00000b7 syscall=6 4 success=yes exit=1 a0=8 a1=ffffe4111718 a2=1 a3=1 items=0 ppid=1 pid=874 auid= 0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm= "(systemd)" exe="/usr/lib/systemd/systemd-executor" subj=kernel key=(null)
[ 21.765845] audit: type=1327 audit(1734996050.855:2): proctitle="(systemd)"
root@am64xx-evm:~#
root@am64xx-evm:~# ifconfig
eth0: flags=4163<UP,BROADCAST,RUNNING,MULTICAST> mtu 1500
inet6 fe80::661c:10ff:fe2f:39df prefixlen 64 scopeid 0x20<link>
ether 64:1c:10:2f:39:df txqueuelen 1000 (Ethernet)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 27 bytes 4942 (4.8 KiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
lo: flags=73<UP,LOOPBACK,RUNNING> mtu 65536
inet 127.0.0.1 netmask 255.0.0.0
inet6 ::1 prefixlen 128 scopeid 0x10<host>
loop txqueuelen 1000 (Local Loopback)
RX packets 58 bytes 5146 (5.0 KiB)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 58 bytes 5146 (5.0 KiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
root@am64xx-evm:~#
// SPDX-License-Identifier: GPL-2.0
/*
* Copyright (C) 2020-2021 Texas Instruments Incorporated - https://www.ti.com/
*/
/dts-v1/;
#include <dt-bindings/phy/phy.h>
#include <dt-bindings/leds/common.h>
#include <dt-bindings/gpio/gpio.h>
#include <dt-bindings/net/ti-dp83867.h>
#include "k3-am642.dtsi"
#include "k3-serdes.h"
/ {
compatible = "ti,am642-evm", "ti,am642";
model = "Texas Instruments AM642 EVM-Config Master board";
chosen {
stdout-path = "serial2:115200n8";
bootargs = "console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000";
};
aliases {
serial2 = &main_uart0;
i2c0 = &main_i2c0;
mmc0 = &sdhci0;
mmc1 = &sdhci1;
ethernet0 = &cpsw_port1;
ethernet1 = &icssg0_emac0;
ethernet2 = &icssg0_emac1;
};
memory@80000000 {
bootph-all;
device_type = "memory";
/* 2G RAM */
reg = <0x00000000 0x80000000 0x00000000 0x80000000>;
};
reserved-memory {
#address-cells = <2>;
#size-cells = <2>;
ranges;
secure_ddr: optee@9e800000 {
reg = <0x00 0x9e800000 0x00 0x01800000>; /* for OP-TEE */
alignment = <0x1000>;
no-map;
};
main_r5fss0_core0_dma_memory_region: r5f-dma-memory@a0000000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa0000000 0x00 0x100000>;
no-map;
};
main_r5fss0_core0_memory_region: r5f-memory@a0100000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa0100000 0x00 0xf00000>;
no-map;
};
main_r5fss0_core1_dma_memory_region: r5f-dma-memory@a1000000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa1000000 0x00 0x100000>;
no-map;
};
main_r5fss0_core1_memory_region: r5f-memory@a1100000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa1100000 0x00 0xf00000>;
no-map;
};
main_r5fss1_core0_dma_memory_region: r5f-dma-memory@a2000000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa2000000 0x00 0x100000>;
no-map;
};
main_r5fss1_core0_memory_region: r5f-memory@a2100000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa2100000 0x00 0xf00000>;
no-map;
};
main_r5fss1_core1_dma_memory_region: r5f-dma-memory@a3000000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa3000000 0x00 0x100000>;
no-map;
};
main_r5fss1_core1_memory_region: r5f-memory@a3100000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa3100000 0x00 0xf00000>;
no-map;
};
mcu_m4fss_dma_memory_region: m4f-dma-memory@a4000000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa4000000 0x00 0x100000>;
no-map;
};
mcu_m4fss_memory_region: m4f-memory@a4100000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa4100000 0x00 0xf00000>;
no-map;
};
rtos_ipc_memory_region: ipc-memories@a5000000 {
reg = <0x00 0xa5000000 0x00 0x00800000>;
alignment = <0x1000>;
no-map;
};
};
/*mdio_mux: mux-controller {
compatible = "gpio-mux";
#mux-control-cells = <0>;
};
mdio_mux_1: mdio-mux-1 {
compatible = "mdio-mux-multiplexer";
mux-controls = <&mdio_mux>;
mdio-parent-bus = <&cpsw3g_mdio>;
#address-cells = <1>;
#size-cells = <0>;
mdio@1 {
reg = <0x1>;
#address-cells = <1>;
#size-cells = <0>;
cpsw3g_phy3: ethernet-phy@3 {
reg = <3>;
};
};
};*/
gpio0: gpio0 {
gpio-controller;
#gpio-cells = <2>;
};
icssg0_eth: icssg0-eth {
compatible = "ti,am642-icssg-prueth";
pinctrl-names = "default";
pinctrl-0 = <&cpuethercatet1100_pins_default>;
sram = <&oc_sram>;
ti,prus = <&pru0_0>, <&rtu0_0>, <&tx_pru0_0>, <&pru0_1>, <&rtu0_1>, <&tx_pru0_1>;
firmware-name = "ti-pruss/am64x-sr2-pru0-prueth-fw.elf",
"ti-pruss/am64x-sr2-rtu0-prueth-fw.elf",
"ti-pruss/am64x-sr2-txpru0-prueth-fw.elf",
"ti-pruss/am64x-sr2-pru1-prueth-fw.elf",
"ti-pruss/am64x-sr2-rtu1-prueth-fw.elf",
"ti-pruss/am64x-sr2-txpru1-prueth-fw.elf";
ti,pruss-gp-mux-sel = <2>, /* MII mode */
<2>,
<2>,
<2>, /* MII mode */
<2>,
<2>;
ti,mii-g-rt = <&icssg0_mii_g_rt>;
ti,mii-rt = <&icssg0_mii_rt>;
ti,iep = <&icssg0_iep0>, <&icssg0_iep1>;
ti,pa-stats = <&icssg0_pa_stats>;
interrupt-parent = <&icssg0_intc>;
interrupts = <24 0 2>, <25 1 3>;
interrupt-names = "tx_ts0", "tx_ts1";
dmas = <&main_pktdma 0xc100 15>, /* egress slice 0 */
<&main_pktdma 0xc101 15>, /* egress slice 0 */
<&main_pktdma 0xc102 15>, /* egress slice 0 */
<&main_pktdma 0xc103 15>, /* egress slice 0 */
<&main_pktdma 0xc104 15>, /* egress slice 1 */
<&main_pktdma 0xc105 15>, /* egress slice 1 */
<&main_pktdma 0xc106 15>, /* egress slice 1 */
<&main_pktdma 0xc107 15>, /* egress slice 1 */
<&main_pktdma 0x4100 15>, /* ingress slice 0 */
<&main_pktdma 0x4101 15>, /* ingress slice 1 */
<&main_pktdma 0x4102 0>, /* mgmnt rsp slice 0 */
<&main_pktdma 0x4103 0>; /* mgmnt rsp slice 1 */
dma-names = "tx0-0", "tx0-1", "tx0-2", "tx0-3",
"tx1-0", "tx1-1", "tx1-2", "tx1-3",
"rx0", "rx1";
ethernet-ports {
#address-cells = <1>;
#size-cells = <0>;
icssg0_emac0: port@0 {
reg = <0>;
phy-handle = <&icssg0_phy1>;
phy-mode = "mii";
/* Filled in by bootloader */
local-mac-address = [00 00 00 00 00 00];
};
icssg0_emac1: port@1 {
reg = <1>;
phy-mode = "mii";
/* Filled in by bootloader */
local-mac-address = [00 00 00 00 00 00];
status = "okay";
fixed-link {
speed = <100>;
full-duplex;
};
};
};
};
};
&main_pmx0 {
am6442mmc1sdcard_pins_default: am6442mmc1sdcard-default-pins {
pinctrl-single,pins = <
AM64X_IOPAD(0x0294, PIN_INPUT, 0) /* (J19) MMC1_CMD */
AM64X_IOPAD(0x028c, PIN_OUTPUT, 0) /* (L20) MMC1_CLK */
AM64X_IOPAD(0x0288, PIN_INPUT, 0) /* (K21) MMC1_DAT0 */
AM64X_IOPAD(0x0284, PIN_INPUT_PULLUP, 0) /* (L21) MMC1_DAT1 */
AM64X_IOPAD(0x0280, PIN_INPUT_PULLUP, 0) /* (K19) MMC1_DAT2 */
AM64X_IOPAD(0x027c, PIN_INPUT_PULLUP, 0) /* (K18) MMC1_DAT3 */
AM64X_IOPAD(0x0298, PIN_INPUT, 0) /* (D19) MMC1_SDCD */
>;
};
am6442uart_pins_default: am6442uart-default-pins {
pinctrl-single,pins = <
AM64X_IOPAD(0x0238, PIN_INPUT, 0) /* (B16) UART0_CTSn */
AM64X_IOPAD(0x023c, PIN_OUTPUT, 0) /* (A16) UART0_RTSn */
AM64X_IOPAD(0x0230, PIN_INPUT, 0) /* (D15) UART0_RXD */
AM64X_IOPAD(0x0234, PIN_OUTPUT, 0) /* (C16) UART0_TXD */
>;
};
mycpsw1_pins_default: mycpsw1-default-pins {
pinctrl-single,pins = <
AM64X_IOPAD(0x011c, PIN_INPUT_PULLDOWN, 4) /* (AA13) PRG1_PRU1_GPO5.RGMII1_RD0 */
AM64X_IOPAD(0x0128, PIN_INPUT_PULLDOWN, 4) /* (U12) PRG1_PRU1_GPO8.RGMII1_RD1 */
AM64X_IOPAD(0x0150, PIN_INPUT_PULLDOWN, 4) /* (Y13) PRG1_PRU1_GPO18.RGMII1_RD2 */
AM64X_IOPAD(0x0154, PIN_INPUT_PULLDOWN, 4) /* (V12) PRG1_PRU1_GPO19.RGMII1_RD3 */
AM64X_IOPAD(0x00d8, PIN_INPUT_PULLDOWN, 4) /* (W13) PRG1_PRU0_GPO8.RGMII1_RXC */
AM64X_IOPAD(0x00cc, PIN_INPUT_PULLDOWN, 4) /* (V13) PRG1_PRU0_GPO5.RGMII1_RX_CTL */
AM64X_IOPAD(0x0124, PIN_OUTPUT_PULLDOWN, 4) /* (V15) PRG1_PRU1_GPO7.RGMII1_TD0 */
AM64X_IOPAD(0x012c, PIN_OUTPUT_PULLDOWN, 4) /* (V14) PRG1_PRU1_GPO9.RGMII1_TD1 */
AM64X_IOPAD(0x0130, PIN_OUTPUT_PULLDOWN, 4) /* (W14) PRG1_PRU1_GPO10.RGMII1_TD2 */
AM64X_IOPAD(0x014c, PIN_OUTPUT_PULLDOWN, 4) /* (AA14) PRG1_PRU1_GPO17.RGMII1_TD3 */
AM64X_IOPAD(0x00e0, PIN_OUTPUT_PULLDOWN, 4) /* (U14) PRG1_PRU0_GPO10.RGMII1_TXC */
AM64X_IOPAD(0x00dc, PIN_OUTPUT_PULLDOWN, 4) /* (U15) PRG1_PRU0_GPO9.RGMII1_TX_CTL */
>;
};
mdio1_pins_default: mdio1-default-pins {
bootph-all;
pinctrl-single,pins = <
AM64X_IOPAD(0x01fc, PIN_OUTPUT, 4) /* (R2) PRG0_PRU1_GPO19.MDIO0_MDC */
AM64X_IOPAD(0x01f8, PIN_INPUT, 4) /* (P5) PRG0_PRU1_GPO18.MDIO0_MDIO */
>;
};
cpuethercatet1100_pins_default: cpuethercatet1100-default-pins {
bootph-all;
pinctrl-single,pins = <
AM64X_IOPAD(0x01a0, PIN_INPUT, 1) /* (U4) PRG0_PRU0_GPO16.PR0_MII_MT0_CLK */
AM64X_IOPAD(0x019c, PIN_OUTPUT, 0) /* (T5) PRG0_PRU0_GPO15.PR0_MII0_TXEN */
AM64X_IOPAD(0x0198, PIN_OUTPUT, 0) /* (V4) PRG0_PRU0_GPO14.PR0_MII0_TXD3 */
AM64X_IOPAD(0x0194, PIN_OUTPUT, 0) /* (R6) PRG0_PRU0_GPO13.PR0_MII0_TXD2 */
AM64X_IOPAD(0x0190, PIN_OUTPUT, 0) /* (AA3) PRG0_PRU0_GPO12.PR0_MII0_TXD1 */
AM64X_IOPAD(0x018c, PIN_OUTPUT, 0) /* (Y3) PRG0_PRU0_GPO11.PR0_MII0_TXD0 */
AM64X_IOPAD(0x0170, PIN_INPUT, 1) /* (AA2) PRG0_PRU0_GPO4.PR0_MII0_RXDV */
AM64X_IOPAD(0x0178, PIN_INPUT, 1) /* (T3) PRG0_PRU0_GPO6.PR0_MII_MR0_CLK */
AM64X_IOPAD(0x016c, PIN_INPUT, 1) /* (V2) PRG0_PRU0_GPO3.PR0_MII0_RXD3 */
AM64X_IOPAD(0x0168, PIN_INPUT, 1) /* (U2) PRG0_PRU0_GPO2.PR0_MII0_RXD2 */
AM64X_IOPAD(0x0174, PIN_INPUT, 1) /* (R3) PRG0_PRU0_GPO5.PR0_MII0_RXER */
AM64X_IOPAD(0x0164, PIN_INPUT, 1) /* (R4) PRG0_PRU0_GPO1.PR0_MII0_RXD1 */
AM64X_IOPAD(0x0160, PIN_INPUT, 1) /* (Y1) PRG0_PRU0_GPO0.PR0_MII0_RXD0 */
AM64X_IOPAD(0x0180, PIN_INPUT, 1) /* (T2) PRG0_PRU0_GPO8.PR0_MII0_RXLINK */
AM64X_IOPAD(0x01f0, PIN_INPUT, 1) /* (AA4) PRG0_PRU1_GPO16.PR0_MII_MT1_CLK */
AM64X_IOPAD(0x01ec, PIN_OUTPUT, 0) /* (U5) PRG0_PRU1_GPO15.PR0_MII1_TXEN */
AM64X_IOPAD(0x01e8, PIN_OUTPUT, 0) /* (U6) PRG0_PRU1_GPO14.PR0_MII1_TXD3 */
AM64X_IOPAD(0x01e4, PIN_OUTPUT, 0) /* (T6) PRG0_PRU1_GPO13.PR0_MII1_TXD2 */
AM64X_IOPAD(0x01e0, PIN_OUTPUT, 0) /* (Y4) PRG0_PRU1_GPO12.PR0_MII1_TXD1 */
AM64X_IOPAD(0x01dc, PIN_OUTPUT, 0) /* (W4) PRG0_PRU1_GPO11.PR0_MII1_TXD0 */
AM64X_IOPAD(0x01c0, PIN_INPUT, 1) /* (W3) PRG0_PRU1_GPO4.PR0_MII1_RXDV */
AM64X_IOPAD(0x01c8, PIN_INPUT, 1) /* (R5) PRG0_PRU1_GPO6.PR0_MII_MR1_CLK */
AM64X_IOPAD(0x01bc, PIN_INPUT, 1) /* (T4) PRG0_PRU1_GPO3.PR0_MII1_RXD3 */
AM64X_IOPAD(0x01b8, PIN_INPUT, 1) /* (V3) PRG0_PRU1_GPO2.PR0_MII1_RXD2 */
AM64X_IOPAD(0x01d8, PIN_INPUT, 1) /* (V6) PRG0_PRU1_GPO10.PR0_MII1_CRS */
AM64X_IOPAD(0x01c4, PIN_INPUT, 1) /* (P4) PRG0_PRU1_GPO5.PR0_MII1_RXER */
AM64X_IOPAD(0x01b4, PIN_INPUT, 1) /* (W2) PRG0_PRU1_GPO1.PR0_MII1_RXD1 */
AM64X_IOPAD(0x01b0, PIN_INPUT, 1) /* (Y2) PRG0_PRU1_GPO0.PR0_MII1_RXD0 */
AM64X_IOPAD(0x01d4, PIN_INPUT, 1) /* (Y5) PRG0_PRU1_GPO9.PR0_MII1_COL */
AM64X_IOPAD(0x01d0, PIN_INPUT, 1) /* (R1) PRG0_PRU1_GPO8.PR0_MII1_RXLINK */
>;
};
mypruicssg0mdio1_pins_default: mypruicssg0mdio1-default-pins {
pinctrl-single,pins = <
AM64X_IOPAD(0x0204, PIN_OUTPUT, 0) /* (P3) PRG0_MDIO0_MDC */
AM64X_IOPAD(0x0200, PIN_INPUT, 0) /* (P2) PRG0_MDIO0_MDIO */
>;
};
main_i2c0_pins_default: main-i2c0-default-pins {
bootph-all;
pinctrl-single,pins = <
AM64X_IOPAD(0x0260, PIN_INPUT, 0) /* (A18) I2C0_SCL */
AM64X_IOPAD(0x0264, PIN_INPUT, 0) /* (B18) I2C0_SDA */
>;
};
mygpio1_pins_default: mygpio1-default-pins {
pinctrl-single,pins = <
AM64X_IOPAD(0x00d0, PIN_OUTPUT, 7) /* (AA7) PRG1_PRU0_GPO6.GPIO0_51 */
AM64X_IOPAD(0x00e4, PIN_OUTPUT, 7) /* (AA8) PRG1_PRU0_GPO11.GPIO0_56 */
>;
};
};
/* uart */
&main_uart0 {
bootph-all;
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&am6442uart_pins_default>;
};
/* eeprom */
&main_i2c0 {
bootph-all;
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&main_i2c0_pins_default>;
clock-frequency = <400000>;
#address-cells = <1>;
#size-cells = <0>;
eeprom@50 {
/* AT24CM01 - default --- ST M24M01-R M24M01-DF - at SCH0402*/
compatible = "st,m24m01-r";
reg = <0x50>;
pagesize = <256>;
/* wp-gpios = <&gpio1 3 0>;*/
num-addresses = <8>;
};
rv3028: rtc@52 {
compatible = "microcrystal,rv3028";
reg = <0x52>;
status = "okay";
trickle-resistor-ohms = <15000>;
};
};
/* eMMC Flash/MMC0 */
&sdhci0 {
status = "okay";
non-removable;
ti,driver-strength-ohm = <50>;
disable-wp;
bootph-all;
};
/* SD/MMC1 */
&sdhci1 {
bootph-all;
status = "okay";
no-1-8-v;
pinctrl-names = "default";
pinctrl-0 = <&am6442mmc1sdcard_pins_default>;
disable-wp;
};
/* Ethernet CPSW */
&cpsw_port1 {
bootph-all;
phy-mode = "rgmii";
phy-handle = <&cpsw3g_phy0>;
reset-gpios = <&gpio0 51 GPIO_ACTIVE_LOW>;
};
&cpsw_port2 {
status = "disabled";
};
&cpsw3g_mdio {
bootph-all;
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&mdio1_pins_default>;
//reset-gpios = <&gpio0 51 GPIO_ACTIVE_LOW>;
//reset-delay-us = <2>;
cpsw3g_phy0: ethernet-phy@0 {
bootph-all;
reg = <0>;
//ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_00_NS>;
//ti,fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>;
};
};
&cpsw3g {
bootph-all;
pinctrl-names = "default";
pinctrl-0 = <&mycpsw1_pins_default>;
/* Map HW8_TS_PUSH to GENF1 */
cpts@3d000 {
ti,pps = <7 1>;
};
};
/* EtCAT ICSSG */
&icssg0_mdio {
bstatus = "okay";
pinctrl-names = "default";
pinctrl-0 = <&mypruicssg0mdio1_pins_default>;
//reset-gpios = <&gpio0 56 GPIO_ACTIVE_LOW>;
//reset-delay-us = <2>;
icssg0_phy1: ethernet-phy@3 {
reg = <0x3>;
};
};
&mailbox0_cluster2 {
status = "okay";
mbox_main_r5fss0_core0: mbox-main-r5fss0-core0 {
ti,mbox-rx = <0 0 2>;
ti,mbox-tx = <1 0 2>;
};
mbox_main_r5fss0_core1: mbox-main-r5fss0-core1 {
ti,mbox-rx = <2 0 2>;
ti,mbox-tx = <3 0 2>;
};
};
&mailbox0_cluster3 {
status = "disabled";
};
&mailbox0_cluster4 {
status = "okay";
mbox_main_r5fss1_core0: mbox-main-r5fss1-core0 {
ti,mbox-rx = <0 0 2>;
ti,mbox-tx = <1 0 2>;
};
mbox_main_r5fss1_core1: mbox-main-r5fss1-core1 {
ti,mbox-rx = <2 0 2>;
ti,mbox-tx = <3 0 2>;
};
};
&mailbox0_cluster5 {
status = "disabled";
};
&mailbox0_cluster6 {
status = "okay";
mbox_m4_0: mbox-m4-0 {
ti,mbox-rx = <0 0 2>;
ti,mbox-tx = <1 0 2>;
};
};
&mailbox0_cluster7 {
status = "disabled";
};
&main_r5fss0_core0 {
mboxes = <&mailbox0_cluster2 &mbox_main_r5fss0_core0>;
memory-region = <&main_r5fss0_core0_dma_memory_region>,
<&main_r5fss0_core0_memory_region>;
};
&main_r5fss0_core1 {
mboxes = <&mailbox0_cluster2 &mbox_main_r5fss0_core1>;
memory-region = <&main_r5fss0_core1_dma_memory_region>,
<&main_r5fss0_core1_memory_region>;
};
&main_r5fss1_core0 {
mboxes = <&mailbox0_cluster4 &mbox_main_r5fss1_core0>;
memory-region = <&main_r5fss1_core0_dma_memory_region>,
<&main_r5fss1_core0_memory_region>;
};
&main_r5fss1_core1 {
mboxes = <&mailbox0_cluster4 &mbox_main_r5fss1_core1>;
memory-region = <&main_r5fss1_core1_dma_memory_region>,
<&main_r5fss1_core1_memory_region>;
};
&mcu_m4fss {
mboxes = <&mailbox0_cluster6 &mbox_m4_0>;
memory-region = <&mcu_m4fss_dma_memory_region>,
<&mcu_m4fss_memory_region>;
};
Here is the ouput of the ping and the command ethtool -S
root@am64xx-evm:~# ip addr add 10.0.10.100/24 dev eth0
root@am64xx-evm:~# ping 10.0.10
ping: connect: Network is unreachable
root@am64xx-evm:~# ping 10.0.10.1
PING 10.0.10.1 (10.0.10.1) 56(84) bytes of data.
From 10.0.10.100 icmp_seq=1 Destination Host Unreachable
From 10.0.10.100 icmp_seq=5 Destination Host Unreachable
From 10.0.10.100 icmp_seq=8 Destination Host Unreachable
From 10.0.10.100 icmp_seq=11 Destination Host Unreachable
^XFrom 10.0.10.100 icmp_seq=14 Destination Host Unreachable
^C
--- 10.0.10.1 ping statistics ---
17 packets transmitted, 0 received, +5 errors, 100% packet loss, time 16372ms
pipe 4
root@am64xx-evm:~# ifconfig
eth0: flags=4163<UP,BROADCAST,RUNNING,MULTICAST> mtu 1500
inet 10.0.10.100 netmask 255.255.255.0 broadcast 0.0.0.0
inet6 fe80::661c:10ff:fe2f:39df prefixlen 64 scopeid 0x20<link>
ether 64:1c:10:2f:39:df txqueuelen 1000 (Ethernet)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 94 bytes 17526 (17.1 KiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
lo: flags=73<UP,LOOPBACK,RUNNING> mtu 65536
inet 127.0.0.1 netmask 255.0.0.0
inet6 ::1 prefixlen 128 scopeid 0x10<host>
loop txqueuelen 1000 (Local Loopback)
RX packets 24 bytes 2858 (2.7 KiB)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 24 bytes 2858 (2.7 KiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
root@am64xx-evm:~# ethtool -s
ethtool: bad command line argument(s)
For more information run ethtool -h
root@am64xx-evm:~# ethtool -S
ethtool: bad command line argument(s)
For more information run ethtool -h
root@am64xx-evm:~# ethtool -S eth0
NIC statistics:
p0_rx_good_frames: 98
p0_rx_broadcast_frames: 37
p0_rx_multicast_frames: 61
p0_rx_crc_errors: 0
p0_rx_oversized_frames: 0
p0_rx_undersized_frames: 0
p0_ale_drop: 0
p0_ale_overrun_drop: 0
p0_rx_octets: 19149
p0_tx_good_frames: 0
p0_tx_broadcast_frames: 0
p0_tx_multicast_frames: 0
p0_tx_octets: 0
p0_tx_64B_frames: 20
p0_tx_65_to_127B_frames: 16
p0_tx_128_to_255B_frames: 40
p0_tx_256_to_511B_frames: 22
p0_tx_512_to_1023B_frames: 0
p0_tx_1024B_frames: 0
p0_net_octets: 19149
p0_rx_bottom_fifo_drop: 0
p0_rx_port_mask_drop: 0
p0_rx_top_fifo_drop: 0
p0_ale_rate_limit_drop: 0
p0_ale_vid_ingress_drop: 0
p0_ale_da_eq_sa_drop: 0
p0_ale_block_drop: 0
p0_ale_secure_drop: 0
p0_ale_auth_drop: 0
p0_ale_unknown_ucast: 0
p0_ale_unknown_ucast_bytes: 0
p0_ale_unknown_mcast: 0
p0_ale_unknown_mcast_bytes: 0
p0_ale_unknown_bcast: 0
p0_ale_unknown_bcast_bytes: 0
p0_ale_pol_match: 0
p0_ale_pol_match_red: 0
p0_ale_pol_match_yellow: 0
p0_ale_mcast_sa_drop: 0
p0_ale_dual_vlan_drop: 0
p0_ale_len_err_drop: 0
p0_ale_ip_next_hdr_drop: 0
p0_ale_ipv4_frag_drop: 0
p0_tx_mem_protect_err: 0
p0_tx_pri0: 0
p0_tx_pri1: 0
p0_tx_pri2: 0
p0_tx_pri3: 0
p0_tx_pri4: 0
p0_tx_pri5: 0
p0_tx_pri6: 0
p0_tx_pri7: 0
p0_tx_pri0_bcnt: 0
p0_tx_pri1_bcnt: 0
p0_tx_pri2_bcnt: 0
p0_tx_pri3_bcnt: 0
p0_tx_pri4_bcnt: 0
p0_tx_pri5_bcnt: 0
p0_tx_pri6_bcnt: 0
p0_tx_pri7_bcnt: 0
p0_tx_pri0_drop: 0
p0_tx_pri1_drop: 0
p0_tx_pri2_drop: 0
p0_tx_pri3_drop: 0
p0_tx_pri4_drop: 0
p0_tx_pri5_drop: 0
p0_tx_pri6_drop: 0
p0_tx_pri7_drop: 0
p0_tx_pri0_drop_bcnt: 0
p0_tx_pri1_drop_bcnt: 0
p0_tx_pri2_drop_bcnt: 0
p0_tx_pri3_drop_bcnt: 0
p0_tx_pri4_drop_bcnt: 0
p0_tx_pri5_drop_bcnt: 0
p0_tx_pri6_drop_bcnt: 0
p0_tx_pri7_drop_bcnt: 0
rx_good_frames: 0
rx_broadcast_frames: 0
rx_multicast_frames: 0
rx_pause_frames: 0
rx_crc_errors: 0
rx_align_code_errors: 0
rx_oversized_frames: 0
rx_jabber_frames: 0
rx_undersized_frames: 0
rx_fragments: 0
ale_drop: 0
ale_overrun_drop: 0
rx_octets: 0
tx_good_frames: 98
tx_broadcast_frames: 37
tx_multicast_frames: 61
tx_pause_frames: 0
tx_deferred_frames: 0
tx_collision_frames: 0
tx_single_coll_frames: 0
tx_mult_coll_frames: 0
tx_excessive_collisions: 0
tx_late_collisions: 0
rx_ipg_error: 0
tx_carrier_sense_errors: 0
tx_octets: 19149
tx_64B_frames: 20
tx_65_to_127B_frames: 16
tx_128_to_255B_frames: 40
tx_256_to_511B_frames: 22
tx_512_to_1023B_frames: 0
tx_1024B_frames: 0
net_octets: 19149
rx_bottom_fifo_drop: 0
rx_port_mask_drop: 0
rx_top_fifo_drop: 0
ale_rate_limit_drop: 0
ale_vid_ingress_drop: 0
ale_da_eq_sa_drop: 0
ale_block_drop: 0
ale_secure_drop: 0
ale_auth_drop: 0
ale_unknown_ucast: 0
ale_unknown_ucast_bytes: 0
ale_unknown_mcast: 0
ale_unknown_mcast_bytes: 0
ale_unknown_bcast: 0
ale_unknown_bcast_bytes: 0
ale_pol_match: 0
ale_pol_match_red: 0
ale_pol_match_yellow: 0
ale_mcast_sa_drop: 0
ale_dual_vlan_drop: 0
ale_len_err_drop: 0
ale_ip_next_hdr_drop: 0
ale_ipv4_frag_drop: 0
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 0
iet_rx_smd_err: 0
iet_rx_frag: 0
iet_tx_hold: 0
iet_tx_frag: 0
tx_mem_protect_err: 0
tx_pri0: 98
tx_pri1: 0
tx_pri2: 0
tx_pri3: 0
tx_pri4: 0
tx_pri5: 0
tx_pri6: 0
tx_pri7: 0
tx_pri0_bcnt: 19149
tx_pri1_bcnt: 0
tx_pri2_bcnt: 0
tx_pri3_bcnt: 0
tx_pri4_bcnt: 0
tx_pri5_bcnt: 0
tx_pri6_bcnt: 0
tx_pri7_bcnt: 0
tx_pri0_drop: 0
tx_pri1_drop: 0
tx_pri2_drop: 0
tx_pri3_drop: 0
tx_pri4_drop: 0
tx_pri5_drop: 0
tx_pri6_drop: 0
tx_pri7_drop: 0
tx_pri0_drop_bcnt: 0
tx_pri1_drop_bcnt: 0
tx_pri2_drop_bcnt: 0
tx_pri3_drop_bcnt: 0
tx_pri4_drop_bcnt: 0
tx_pri5_drop_bcnt: 0
tx_pri6_drop_bcnt: 0
tx_pri7_drop_bcnt: 0
root@am64xx-evm:~#
Hope i gave enough details to find the problem.