This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5718: How to mirror an SD card system to EMMC Flash with relatively simple operation steps

Part Number: AM5718


Tool/software:

Hello experts:

       I use TI's am5718 as the processor, SDK version: ti-processor-sdk-linux-am57xx-evm-04.03.00.05.

       Now I can boot from the SD card, and the file system is also on the SD card.Due to the use of this product in car devices, considering vibration issues, it is necessary to mirror the SD system to the EMMC interface flash. 

       Our board has QSPI and emmcFlash, and we hope to boot from QSPI with the file system in emmcFlash. I am now able to implement QSPI startup and file system implementation in emmcFlash。I completely created the system for emmcFlash based on SD card partitioning.

       Because factory production is required,Partitioning hard drives and creating systems are too complex and time-consuming.

       Is there a simple way to mirror the SD card system to EMMCFlash?

       Perhaps my poor English skills prevented me from finding the ideal answer on the forum. Do experts have any good solutions or suggestions?

        Thank you very much!