Part Number: AM5728
Other Parts Discussed in Thread: TFP401
Tool/software:
Hi,
I have a custom AM5278 board and with TI-sdk ti-processor-sdk-linux-am57xx-evm-05.03.00.07 which is similar to the EVM board, here we have connected the vin3a-0 to vin3a-23 to a TFP401 decoder.
the issue we face is as below 
we had checked the TFP401 output which goes to the board and can confirm that TFP401 is giving out RGB format properly , but when launched in our system through either GST command or the application that was made we face the above issue.
Also this issue occurs only for a solid color of pure black(0,0,0) on white or white on black where ever black is there the pixel on that horizontal line shift to the right causing this issue , in case we reduce the color of the black by (20,20,20) this issue is not observed and everything looks normal.
we also launched the test pattern as below shown but it did not show any problem with the same.
the below image is the real test pattern image

Could you help us solve the issue as we think it might be an issue with the Processor for rendering the received RGB format.
Regards ,
Roshan Rajagopal