Part Number: AM5716
Tool/software:
Hi :
I use the AM571X processor of your company, and the sdk is 9.03. When I use the sd card to boot, it is normal and I can enter the kernel, while when I use the emmc, it has been formatted and well distinguished, but the startup fails. When I enter the uboot, I can either press the command or load it into the kernel and device tree. Any reply and guidance would be greatly appreciated

=> setenv mmcdev 1
=> setenv bootpart 1:2
=> setenv mmcroot /dev/mmcblk1p2 rw
=>
=>
=> run mmcboot
switch to partitions #0, OK
mmc1(part 0) is current device
SD/MMC found on device 1
Failed to load '/boot/'
=>
=> load mmc 1:2 0x82000000 /boot/zImage
8393216 bytes read in 102 ms (78.5 MiB/s)
=> load mmc 1:2 0x88000000 /boot/am571x-idk.dtb
213917 bytes read in 5 ms (40.8 MiB/s)
=>
=>
=> run mmcboot
switch to partitions #0, OK
mmc1(part 0) is current device
SD/MMC found on device 1
Failed to load '/boot/'
=>
=>
=> bootz 0x82000000-0x88000000
Kernel image @ 0x82000000 [ 0x000000 - 0x801200 ]
Working FDT set to 0
FDT and ATAGS support not compiled in
resetting ...