Other Parts Discussed in Thread: AM3517
Hello everyone,
I'm trying to use Platform Builder to build an OS image of Windows 7 CE Embedded for the AM3517 EVM. I need to be able to use the I2C and mcSPI devices as well as configure my device's OTG port. After selecting to include the I2C bus driver with Platform Builder and building the image I do not see the supporting DLLs in the image. The same seems to be true of the SPI driver. The I2C Bus Driver Properties indicate the inclusion of the SYSGEN_I2C Sysgen Variable. Windows Embedded Test Kit indicates I need to include a BSP variable, BSP_I2CBUS1. I don't know how to include this. It would probably solve my problem with the I2C. Anyone know how I can set that? Any help would be greatly appreciated.
If anyone could point me to some documentation for configuring the OS Design to get the SPI device included and to configure and customize the functionality of the OTG port that would be cool too.
David