Other Parts Discussed in Thread: SYSCONFIG, SK-AM62-LP
Tool/software:
Hi,
My customer has a question for power rail configuration in Linux SDK.
There are some differences in voltages in each power rail on the customer's board.
He found there is SysConfig tool available to configure some of these power rails, but he wants to change them manually in the code.
Here is a table shows differences between SK-AM62LP and the custom board.
TI System Configuration Tool Available | Power rail | SK-AM62LP Configuration |
Custom board Configuration |
Yes | VDDSHV0 | 3.3V | 3.3V |
Yes | VDDSHV1 | 1.8V | 3.3V |
Yes | VDDSHV2 | 3.3V | 3.3V |
Yes | VDDSHV3 | 3.3V | 3.3V |
Yes | VDDSHV4 | 1.8V | 1.8V |
Yes | VDDHSV5 | 3.3V/1.8V | 3.3V/1.8V |
Yes | VDDSHV6 | 1.8V | 3.3V |
Yes | VDDSHV_MCU | 3.3V | 3.3V |
Yes | VDDSHV_CANUART | 3.3V | 3.3V |
- | VDDA_TEMP0 | 1.8V | 1.8V |
- | VDDA_TEMP1 | 1.8V | 1.8V |
- | VDDA_PLL | 1.8V | 1.8V |
- | VDDA_DDR_PLL0 | 0.75V | NA |
- | VDDA_MCU | 1.8V | 1.8V |
- | VDDA_1P8_OLDI0 | 1.8V | 1.8V |
- | VDDA_1P8_OLDI0 | 1.8V | 1.8V |
- | VDDA_CORE_USB | 0.75V | 0.75V |
- | VDDA_CORE_CSIRX0 | 0.75V | 0.75V |
- | DDA_1P8_CSIRX0 | 1.8V | 1.8V |
Yes | VDDA_1P8_USB | 1.8V | 1.8V |
Yes | VDDA_3P3_USB | 3.3V | 3.3V |
- | VDD_CORE | 0.75V | 0.75V |
- | VDDR_CORE | 0.85V | 0.85V |
Yes | VDDS_DDR | 1.1V | 1.1V |
Yes | VDDS_OSC0 | 1.8V | 1.8V |
Yes | VDDS_DDR_C | 1.1V | 1.1V |
- | VDD_CANUART | 3.3V | 0.75V |
- | VPP | 1.8V | NC |
In which code, the customer should change to configure above differences?
Thanks and regards,
Koichiro Tashiro