This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: J722S2 C7x clock frequency change

Part Number: TDA4VM


Tool/software:

Dear Ti expert

I am trying to change the C7x clock frequency.

The purpose is to meet the speed grade J. For the J grade, the C7x should be 912.5 MHz.

#1.  Changed the code
       mcu_plus_sdk_j722s_09_02_00_41/source/drivers/bootloader/soc/j722s/bootloader_soc.c
          
{ /* CSL_CORE_ID_C75SS0_0 */
.tisciProcId = SCICLIENT_PROC_ID_C7X256V0_C7XV_CORE_0,
.tisciDevId = TISCI_DEV_C7X256V0_C7XV_CORE_0,
.tisciClockId = TISCI_DEV_C7X256V0_C7XV_CORE_0_C7XV_CLK,
//.defaultClockHz = (uint32_t)(1000*1000000),
.defaultClockHz = (uint32_t)(912.5*1000000),   // default value is (uint32_t)(1000*1000000),
.coreName = "c75ss0-0",
},

{ /* CSL_CORE_ID_C75SS1_0 */
.tisciProcId = SCICLIENT_PROC_ID_C7X256V1_C7XV_CORE_0,
.tisciDevId = TISCI_DEV_C7X256V1_C7XV_CORE_0,
.tisciClockId = TISCI_DEV_C7X256V1_C7XV_CORE_0_C7XV_CLK,
//.defaultClockHz = (uint32_t)(1000*1000000),
.defaultClockHz = (uint32_t)(912.5*1000000),  // default value is (uint32_t)(1000*1000000),
.coreName = "c75ss1-0",
},

-------------------------------------------------
 It did not work.

--------------------------------------------------------

#2. Using k3conf

         k3conf set clock 208 0 912500000

   k3conf set clock 268 0 912500000

 

-------------------------------------------------
 It did not work.
error with Invalid clock arguments

--------------------------------------------------------

Please give us guide to solve the problem.

Thank you.

Sincerely
Sukwon Kim