Part Number: TDA4VM
Tool/software:
I'm evaluating the SDE on TDA4VM, mostly by means of the edgeai-gst-plugins (https://github.com/TexasInstruments/edgeai-gst-plugins/tree/main)
Going through the accelerator capabilities, it's stated that the Disparity search range (SR) can be of 64, 128 or 192, and a gst-inspect of tiovxsde reveals the existance of the disparity-max parameter:
disparity-max: Maximum Disparity
flags: readable, writable, controllable, changeable only in NULL or READY state
Enum "GstTIOVXSdeMaxDisparity" Default: 0, "disparity_max_63"
(0): disparity_max_63 - disparity_min +63
(1): disparity_max_127 - disparity_min +127
(2): disparity_max_191 - disparity_min +191
With the following pipeline everything works fine:
gst-launch-1.0 \
filesrc location=im0.png ! decodebin ! videoconvert ! imagefreeze ! video/x-raw, format=NV12 ! queue ! sde.left_sink \
filesrc location=im1.png ! decodebin ! videoconvert ! imagefreeze ! video/x-raw, format=NV12 ! queue ! sde.right_sink \
tiovxsde name=sde disparity-max=0 ! tiovxsdeviz ! pngenc snapshot=TRUE ! filesink location=tda4vm_stereo.png 2>&1
However, when I try to change the disparity-max=0 to some other value (e.g. disparity-max=1), the pipeline fails with the following errors:
234008.651009 s: VX_ZONE_INIT:Enabled
234008.651055 s: VX_ZONE_ERROR:Enabled
234008.651096 s: VX_ZONE_WARNING:Enabled
234008.651695 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target MPU-0
234008.651918 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target MPU-1
234008.652071 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target MPU-2
234008.652224 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target MPU-3
234008.652284 s: VX_ZONE_INIT:[tivxInitLocal:136] Initialization Done !!!
234008.653134 s: VX_ZONE_INIT:[tivxHostInitLocal:101] Initialization Done for HOST !!!
Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...
234008.850413 s: VX_ZONE_ERROR:[ownContextSendCmd:875] Command ack message returned failure cmd_status: -1
234008.850441 s: VX_ZONE_ERROR:[ownNodeKernelInit:590] Target kernel, TIVX_CMD_NODE_CREATE failed for node node_126
234008.850467 s: VX_ZONE_ERROR:[ownNodeKernelInit:591] Please be sure the target callbacks have been registered for this core
234008.850486 s: VX_ZONE_ERROR:[ownNodeKernelInit:592] If the target callbacks have been registered, please ensure no errors are occurring within the create callback of this kernel
234008.850505 s: VX_ZONE_ERROR:[ownGraphNodeKernelInit:608] kernel init for node 0, kernel com.ti.hwa.dmpac_sde ... failed !!!
234008.850526 s: VX_ZONE_ERROR:[vxVerifyGraph:2159] Node kernel init failed
234008.850543 s: VX_ZONE_ERROR:[vxVerifyGraph:2213] Graph verify failed
234008.850643 s: VX_ZONE_ERROR:[ownReleaseReferenceInt:598] Invalid reference
Is there something i'm not understanding? With the default disparity close objecs are badly predicted:

Additional info:
- I'm using the the PROCESSOR-SDK-LINUX-SK-TDA4VM prebuilt .wic image (version 09.02.00.05)
- tiovx plugin version: 0.7.0
Thanks,
Loris