hi,
I am using TMDSEVM L138 board for proccessing PAL video.
The datasheet says :
"2.1 Clock Control
The VPIF has 4 clock input pins and 2 clock output pins. Each channel has 1 clock input pin with clock edge control using the CLKEDGE bit in the channeln control register (Cn CTRL). VPIF can provide a clock for an external device on channel 2 or 3 using the CLKEN bit in the appropriate C2CTRL or C3CTRL register. The clock generated by VPIF will have the same frequency as the input clock."
However, the output video signal is "slide" relative to the input signal. That is, has a output frequency different from the input.
This creates problems when i synchronize the process of image processing and video output.
How to solve this problem?
Vladimir.