This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HW multiplex for SD video chanels for NETRA



Hello

I am  trying to figure out how to multiplex 8 SD channel per one VIP.

Suppose FPGA glue logic is not an issue, can it be done in the following manner:

·         Using two pixel clocks per VIP and dividing the 16 bit busses into two 8 bit busses, as suggested on Table 2-6.

·         Multiplex 4 channels with embedded sync and identical resolution as required on each bus.

Suppose this is possible, can each of the two 8 bit busses be configured to a different SD resolution?

If it cannit be done in that manner, is it possible at all?

thanks