Tool/software:
Hi TI,
I have a few questions regarding the security accelerators (SA2UL/SA3UL) on the AM62Ax platform:
1.Driver Availability:
In the HSM-Care Package, I see that the only driver provided is for SA2UL. However, in the MCU+SDK, there are examples for SA3UL but no mention of SA2UL. Could you clarify why there are separate driver implementations between these two packages?
2.Hardware vs. Driver Differences:
According to the "K3 Processor Security Accelerator" document, the AM62Ax is listed as having the SA3p1_UL. Could you explain whether the difference between SA2UL and SA3UL is at the hardware level, or if it's simply a matter of different driver implementations?
3.AM62Ax SA Version:
Can you confirm whether the AM62Ax uses SA3UL or SA2UL? There seems to be some ambiguity across the available documentation and SDK.
4.Support for Chinese Algorithms:
The documentation mentions that the SA supports SM2, SM3, and SM4 algorithms. However, the current drivers do not appear to provide implementation or access to these resources. Is there a timeline for when these will be available?
Thank you in advance for your clarification.
Regards,
Yang