This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VE-Q1: TDA4VE EVM is not bootable if tiboot3.bin is replaced with the built one

Part Number: TDA4VE-Q1
Other Parts Discussed in Thread: TDA4VM

Tool/software:

Hi TI experts,

On the TDA4VM EVM, it is bootable if I replace /BOOT/tiboot3.bin with the one I build from Linux SDK (r85)

But on TDA4VE EVM, it fails to boot (without any UART output) if /BOOT/tiboot3.bin is replaced with the one I build from Linux SDK (r85)

How can I make the r5 tiboot3.bin file that I built work properly on the TDA4VE?

Thanks,

Regards,

Christopher