This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VL-Q1: MMCSD driver: set pSLC mode for eMMC

Part Number: TDA4VL-Q1

Tool/software:

Dear TI-Support,

I am currently accessing the eMMC via the SBL bootloader using the MMCSD(_v2) driver. Is there any way to enable pSLC mode for the eMMC using the MMCSD driver?

If not, which eMMC command can I use to write certain values of the ECSD register? Do you have any example of pSLC mode activation via SBL?

Best regards,

Andreas

  • Hi Andreas,

    Is there any way to enable pSLC mode for the eMMC using the MMCSD driver?

    Currently,it is not present in the MMCSD driver . Since this option is only one-time configurable,it is better to rather configure it from either UBOOT or linux kernel.

    If not, which eMMC command can I use to write certain values of the ECSD register? Do you have any example of pSLC mode activation via SBL?

    Configuring PSLC in Linux kernel using mmc-util:

    Command : [mmc enh_area --help] command in the userspace of linux kernel.

    Configuring PSLC in UBOOT:

    1:Enter into Linux kernel,execute the following command ,and just note it down:

       > cat /sys/class/block/mmcblk0/size

       It basically indicates the number of 512 blocks present in the emmc uda partition

    2:Reboot into Uboot and enter the below command which will just test if it is working:

    > mmc hwpartition user enh <start> <number of 512B sized blocks> check

    SYNTAX:



    I am attaching an example below just for reference:

    Here 62160896 is the value obtained after running cat /sys/class/block/mmcblk0/size as stated earlier.

    Here 1264 indicates the maximum number of HC WP Group Size(8Mib(as in the below image)) blocks allowed.

    Hence number of 512B sized blocks now = (1264×8×1024×1024)/512 which is equal to 20709376 which works fine.


    3:Now to set this configuration permanently:
    NOTE:Because all the operations are one-time only,be very careful before applying the below command.
     > mmc hwpartition user enh 0 20709376 wrrel on complete

    4:Power cycle the board for the changes to get applied.
     
  • Hi Gokul,

    I was able to perform this change manually in the SBL by utilizing the MMCSD_v2_transfer() function.

    One last question for this topic: Do you have an idea how long it takes the eMMC to apply these changes after a powercycle? Does the SBL wait for finalization of the pSLC mode when initializing the eMMC with MMCSD_init()?

    best regards,

    Andreas

  • Hi Andreas,

    Do you have an idea how long it takes the eMMC to apply these changes after a powercycle?

    Ideally ,as soon as you power cycle the board,the changes should take effect.

    Does the SBL wait for finalization of the pSLC mode when initializing the eMMC with MMCSD_init()?

    Since there is no implementation of pSLC mode in SBL , it will not wait  when initializing the eMMC init.