This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Issues running CSL USB Poll Example

I’m trying to run the CSL USB Poll Example on my C5505, and I’m having trouble getting the PC side of the project to work.  I’ve gotten the example code running on my board, but the instructions for the PC side say:

 

“This USB test can be verified by a host USB tool (c5505usb_ep_diag.exe) which can send or receive 64 bytes of data to the USB device. This tool should be installed on the host PC. This tool requires Jungo USB driver which can be downloaded from the link www.jungo.com. inf file should be installed for the C5505/C5515 USB device using driver wizard of the windriver.”

 

I downloaded and installed WinDriver, but the driver wizard has no option to install a .inf file.  Also, my C5505 board doesn’t show up in WinDriver’s list of USB devices, so I’m not sure how I would install the .inf file anyways.  Any help would be greatly appreciated!