Tool/software:
Hi TI Support Team,
I am trying to display the product logo from the U-Boot loader on the custom board AM6422. I have configured the SPI device driver in U-Boot to communicate with the spi-LCD. However, I am encountering an issue when trying to initialize and access the SPI slave device (using spi_get_bus_and_cs), causing U-Boot to hang. Please let me know if I have missed any necessary configurations.
CONFIG_SPI=y
CONFIG_DM_SPI=y
CONFIG_CMD_SPI=y
Changes in k3-am642-evm.dts
main_spi0_pins_default: main-spi0-pins-default {
pinctrl-single,pins = <
AM64X_IOPAD(0x0210, PIN_INPUT, 0) /* (D13) SPI0_CLK */
AM64X_IOPAD(0x0208, PIN_OUTPUT, 0) /* (D12) SPI0_CS0 */
AM64X_IOPAD(0x0214, PIN_OUTPUT, 0) /* (A13) SPI0_D0 */
>;
};
&main_spi0 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&main_spi0_pins_default>;
ti,pindir-d0-out-d1-in = <1>;
ti,spi-num-cs = <1>;
spidev@0 {
status = "okay";
compatible = "rohm,dh2228fv";
spi-max-frequency = <5000000>;
reg = <0>;
spi-cs-high;
};
};
Uboot Debug Log:

Regards,
Kalyan