Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi Ti expert
Board: custom board
SDK: 0806
I now want to use spi devices in linux(main_spi1 main_spi2). I referred to this document: e2e.ti.com/.../faq-ccs-tda4vm-how-to-use-spi-spi_dev-on-tda4-j721e
but I found in the actual test that clk does not have a waveform.
The following is my configuration:



This is in linux:

But the clk pin has no waveform, and spi has mounted sub-devices (both two spis have sub-devices, and the clk pin has no waveform).
I have checked all the pins and there are no conflicts.
I also tested on the tda4_evm board, and there is no waveform on the clk pin.
The clk pin I tested using an oscilloscope。
How can I solve this problem?
Best Regards
Eason