This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 SDK Supported Ethernet PHYs

Hi,

What ethernet PHYs are currently supported in the DM8148 development sdk?  Right now we are using a MIstral SDK which contains AR8031.  Are other PHYs supported?  I understand the software driver could be modified to support others but am wondering whats available currently.

  • Hi

    The PHY driver currently used for handling the AR8031 is a generic PHY layer implementation under Linux and should be able to work with most standard PHYs without any changes - sufficient care must be taken with the HW interfacing to ensure any timing restrictions imposed by the PHy are complied with