Part Number: AM5728
Tool/software:
Hi,
How can I build and test an AM57xx driver example Using CCS?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The FAQ contains Windows and Linux scripts used to create example CCS projects for all PDK sub-components. The following steps describe how to create CCS example project and run them on targets.
1. Project Creation
2. Project Build
3. Run Program
Prerequisites:
Step 1:
Windows: Update CCS version in pdkProjectCreate.bat file in case different CCS version is used.
Path : <SDK Root>\pdk_[soc]_[version]\packages
set CCS_INSTALL_PATH=C:\ti\ccs1271\ccs
Linux : Update CCS version in pdkProjectCreate.sh file in case different CCS version is used.
Path : <SDK Root>/pdk_[soc]_[version]/packages
export CCS_INSTALL_PATH=~/ti/ccs1271/ccs
Step 2:
Need to add the path in CSS: Please refer to the link below for this step
Example: From CCS, select Window -> Preferences->Code Composer Studio -> RTSC -> Products
Step 3:
Create new target configuration in CCS: Please refer to the link below for this step
Note:- For AM57xx, select the option below
Connection: Texas Instruments XDS100v2 USB Debug Probe
Board or Device: IDK_AM572x / EVM_AM572x / IDK_AM571x / IDK_AM574x
Step 4:
If you connect to the EVM UART, use the following host configuration:
Baud Rate : 115200
Data Bits : 8
Parity : None
Flow Control : Off
1.Project Creation:
step 1:
Run the pdksetupenv script to setup the PDK and SDK path variables
Windows:
<SDK Root>\pdk_[soc]_[version]\packages\ pdksetupenv.bat
Linux:
<SDK Root>/pdk_[soc]_[version]/packages$ source pdksetupenv.sh
Step 2:
Run the pdkProjectCreate script. The script takes parameters for creating projects for different configurations. Below are the command formats for Windows pdkProjectCreate.bat and Linuxs pdkProjectCreate.sh
Windows Usage:
pdkProjectCreate.bat [soc] [board] [endian] [module] [project type] [processor] [pdkDir]
Linux Usage:
./pdkProjectCreate.sh [soc] [board] [endian] [module] [project type] [processor]
Description: (first option is default)
soc - AM571x / AM572x / AM574x
board - all (use "all"SOCs)
-or-
Refer to SDK Root>\pdk_[soc]_[version]\packages\ti\board\lib
for valid board inputs for the soc's
endian - little / big
module - all
-or-
csl / emac / gpio / i2c / icss_emac / mcasp / mmcsd /
pcie / pm / pruss / spi / uart / usb / vps / osal
project type - all / example / test
processor - arm / dsp / ipu
pdkDir - This File Location "<SDK Root>\pdk_[soc]_[version]\packages"
pdkProjectCreate.bat AM572x idkAM572x little
- Creates all module projects for idkAM572x device for arm little endian
Example:
pdkProjectCreate.bat AM572x idkAM572x little gpio all dsp
./pdkProjectCreate.sh AM572x idkAM572x little gpio all dsp
Note:-
The script creates all the projects available for given configurations. Default location of the projects created is at <SDK Root>/pdk_[soc]_[version]/packages/MyExampleProjects
2.Project Build:
Steps to run example projects on A15/C66x/M4 Targets
Import Project:
Below are the steps for importing project
1.Open CSS -> Click on File -> Import
2.On the Import Dialog Box select Existing CCS Project
3.Click on Next
4.This will pop up a new dialog box; ensure that ‘Select Root Directory’ option is selected
5.Click on Browse and select the top level directory where the project is present.
For example : <SDK Root>\pdk_[soc]_[version]\packages\MyExampleProjects
6.Under the projects section you should see the project
For Example:
GPIO_LedBlink_idkAM572x_m4TestProject
7.Click Finish
Note:-
To build the project; ensure that the project you want to build,
i.e., GPIO_LedBlink_idkAM572x_m4TestProject is set as the active project. Click on Project -> Build Active Project, Naming convention of Projects created.
Example:
GPIO_LedBlink_idkAM572x_m4TestProject
3.Run Project:
There are no boot switches to set up for emulation mode on the AM572x EVM. When you put in the SD card, the evm switches from emulator mode to SD boot mode. By default, the evm is in emulation boot mode.
1.Launch the CCS
2.Launch Target configuration
3.To execute the program ensure the following is done
AM572x is an ARM master boot device so connect to the A15_0 first
For A15 Target:
1.Click on Target (A15)-> Connect -> Reset CPU
2.Click on Target (A15) -> Load Program
3.Select the executable file to be loaded
Example:
<SDK Root>\pdk_[soc]_[version]\packages\MyExampleProjects\GPIO_LedBlink_idkAM572x_armTestProject\Debug\GPIO_LedBlink_idkAM572x_armTestProject.out
For C66x Target:
1.Click on Target (A15)-> Connect -> Reset CPU
2.Click on Target (C66x) -> Connect ->Load Program
3.Select the executable file to be loaded
Example:
<SDKRoot>\pdk_[soc]_[version]\packages\MyExampleProjects\GPIO_LedBlink_idkAM572x_c66xTestProject\Debug\GPIO_LedBlink_idkAM572x_c66xTestProject.out
For M4 Target:
1.Click on Target (A15)-> Connect -> Reset CPU
2.Click on Target (M4) -> Connect ->Load Program
3.Select the executable file to be loaded
Example:
<SDK Root>\pdk_[soc]_[version]\packages\MyExampleProjects\GPIO_LedBlink_idkAM572x_m4TestProject\Debug\GPIO_LedBlink_idkAM572x_m4TestProject.out
4.Click on OK
5.Once the project is loaded
click on Target -> Run to execute it
Regards,
Karthik