Tool/software:
Hi Tier:
I want to install igh ethercat to am62p, but failed.
SDK:tisdk-default-image-rt-am62pxx-evm-10.01.10.04.rootfs.wic
Board:AM62P
IGH ETHERCAT:ethercat-stable-1.6
configure: error: Failed to find Linux sources. Use --with-linux-dir!
root@am62pxx-evm:/media/ethercat-stable-1.6#
root@am62pxx-evm:/media/ethercat-stable-1.6#
root@am62pxx-evm:/media/ethercat-stable-1.6#
root@am62pxx-evm:/media/ethercat-stable-1.6#
root@am62pxx-evm:/media/ethercat-stable-1.6#
root@am62pxx-evm:/media/ethercat-stable-1.6#
root@am62pxx-evm:/media/ethercat-stable-1.6#
root@am62pxx-evm:/media/ethercat-stable-1.6#
root@am62pxx-evm:/media/ethercat-stable-1.6#
root@am62pxx-evm:/media/ethercat-stable-1.6#
root@am62pxx-evm:/media/ethercat-stable-1.6#
root@am62pxx-evm:/media/ethercat-stable-1.6#
root@am62pxx-evm:/media/ethercat-stable-1.6#
root@am62pxx-evm:/media/ethercat-stable-1.6#
root@am62pxx-evm:/media/ethercat-stable-1.6#
root@am62pxx-evm:/media/ethercat-stable-1.6#
root@am62pxx-evm:/media/ethercat-stable-1.6#
root@am62pxx-evm:/media/ethercat-stable-1.6# ./configure
checking for a BSD-compatible install... /usr/bin/install -c
checking whether build environment is sane... yes
checking for a thread-safe mkdir -p... /usr/bin/mkdir -p
checking for gawk... gawk
checking whether make sets $(MAKE)... yes
checking whether make supports nested variables... yes
checking whether make supports nested variables... (cached) yes
checking for a sed that does not truncate output... /usr/bin/sed
checking for pkg-config... /usr/local/bin/pkg-config
checking pkg-config is at least version 0.9.0... yes
checking whether make supports the include directive... yes (GNU style)
checking for gcc... gcc
checking whether the C compiler works... yes
checking for C compiler default output file name... a.out
checking for suffix of executables...
checking whether we are cross compiling... no
checking for suffix of object files... o
checking whether we are using the GNU C compiler... yes
checking whether gcc accepts -g... yes
checking for gcc option to accept ISO C89... none needed
checking whether gcc understands -c and -o together... yes
checking dependency style of gcc... gcc3
checking for ar... ar
checking the archiver (ar) interface... ar
checking for g++... g++
checking whether we are using the GNU C++ compiler... yes
checking whether g++ accepts -g... yes
checking dependency style of g++... gcc3
checking build system type... aarch64-unknown-linux-gnu
checking host system type... aarch64-unknown-linux-gnu
checking how to print strings... printf
checking for a sed that does not truncate output... (cached) /usr/bin/sed
checking for grep that handles long lines and -e... /usr/bin/grep
checking for egrep... /usr/bin/grep -E
checking for fgrep... /usr/bin/grep -F
checking for ld used by gcc... /usr/aarch64-oe-linux/bin/ld
checking if the linker (/usr/aarch64-oe-linux/bin/ld) is GNU ld... yes
checking for BSD- or MS-compatible name lister (nm)... /usr/bin/nm -B
checking the name lister (/usr/bin/nm -B) interface... BSD nm
checking whether ln -s works... yes
checking the maximum length of command line arguments... 1572864
checking how to convert aarch64-unknown-linux-gnu file names to aarch64-unknown-linux-gnu format... func_convert_file_noop
checking how to convert aarch64-unknown-linux-gnu file names to toolchain format... func_convert_file_noop
checking for /usr/aarch64-oe-linux/bin/ld option to reload object files... -r
checking for file... file
checking for objdump... objdump
checking how to recognize dependent libraries... pass_all
checking for dlltool... no
checking how to associate runtime and link libraries... printf %s\n
checking for archiver @FILE support... @
checking for strip... strip
checking for ranlib... ranlib
checking command to parse /usr/bin/nm -B output from gcc object... ok
checking for sysroot... no
checking for a working dd... /usr/bin/dd
checking how to truncate binary pipes... /usr/bin/dd bs=4096 count=1
checking for mt... no
checking if : is a manifest tool... no
checking how to run the C preprocessor... gcc -E
checking for ANSI C header files... yes
checking for sys/types.h... yes
checking for sys/stat.h... yes
checking for stdlib.h... yes
checking for string.h... yes
checking for memory.h... yes
checking for strings.h... yes
checking for inttypes.h... yes
checking for stdint.h... yes
checking for unistd.h... yes
checking for dlfcn.h... yes
checking for objdir... .libs
checking if gcc supports -fno-rtti -fno-exceptions... no
checking for gcc option to produce PIC... -fPIC -DPIC
checking if gcc PIC flag -fPIC -DPIC works... yes
checking if gcc static flag -static works... no
checking if gcc supports -c -o file.o... yes
checking if gcc supports -c -o file.o... (cached) yes
checking whether the gcc linker (/usr/aarch64-oe-linux/bin/ld) supports shared libraries... yes
checking whether -lc should be explicitly linked in... no
checking dynamic linker characteristics... GNU/Linux ld.so
checking how to hardcode library paths into programs... immediate
checking whether stripping libraries is possible... yes
checking if libtool supports shared libraries... yes
checking whether to build shared libraries... yes
checking whether to build static libraries... yes
checking how to run the C++ preprocessor... g++ -E
checking for ld used by g++... /usr/aarch64-oe-linux/bin/ld
checking if the linker (/usr/aarch64-oe-linux/bin/ld) is GNU ld... yes
checking whether the g++ linker (/usr/aarch64-oe-linux/bin/ld) supports shared libraries... yes
checking for g++ option to produce PIC... -fPIC -DPIC
checking if g++ PIC flag -fPIC -DPIC works... yes
checking if g++ static flag -static works... no
checking if g++ supports -c -o file.o... yes
checking if g++ supports -c -o file.o... (cached) yes
checking whether the g++ linker (/usr/aarch64-oe-linux/bin/ld) supports shared libraries... yes
checking dynamic linker characteristics... (cached) GNU/Linux ld.so
checking how to hardcode library paths into programs... immediate
checking whether to build kernel modules... yes
configure: error: Failed to find Linux sources. Use --with-linux-dir!
but in /lib/modules/6.6.58-rt45-ti-rt-01780-gc79d7ef3a56f-dirty, only have:
root@am62pxx-evm:/lib/modules/6.6.58-rt45-ti-rt-01780-gc79d7ef3a56f-dirty# ls
kernel modules.builtin.bin modules.order
modules.alias modules.builtin.modinfo modules.softdep
modules.alias.bin modules.dep modules.symbols
modules.builtin modules.dep.bin modules.symbols.bin
modules.builtin.alias.bin modules.devname updates
And the board can not connet Internet.
thx