Hi,
We are feeding analog video input (PAL-720X576) in DM6446 EV board and video output is 800x600 LCD display. We are using the custom application to execute the analog input video to play it into our LCD display. Now the problem is, We got the 800x600 lcd display out but if I run the application to execute the analog video input,it is not opened.
In initial days we used analog video input and analog video output which we feed it into lcd controller of the LCD display, Everything worked well. We got the analog input video into our display while executing the application.
We are taking RGB (24bit) and HSYNC ,VSYNC from dm6446 and feeding it to our LCD . We are getting the perfect 800x600 resolution display. But we are not able to get the analog video input to play in our LCD display, What changes i have to do to get the analog camera video input to play in our LCD display ? Video camera input is 720x576 analog video and display out is 800x600 digital resolution. How do we synchronized both the signal?
Does it require any register setting and hardware wiring? if yes, kindly provide those information?
Thanks in advance.