This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Reset reason when board reset automatically

Part Number: TDA4VM


Tool/software:

Dear TI.

We made a test board and it reset automatically within 10 minute.

When it reboot with SD mode.

In uboot prompt, WKUP_CTRL_MMR0_CFG0 at 0x43018178 is like below.

> md.l 0x43018178 1

43018178: 00010001

Is there another register which I could check why this reset is triggered ? (Watchdog or something)

Strangely, when it boot in EMMC mode, it can not reboot but lock-up (console does not respond)

I suspect that reset was triggered automatically, but it could not reboot.

When I executed reboot command in linux console, it could not reboot.

FYI, I'm using ti-processor-sdk-linux-j7200-evm-09_02_00_04.

BR

Jace