This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: TDA4VM Development Support

Part Number: TDA4VM

Tool/software:

Due to the project, we need the following assistance:

  1. If the NOR Flash model connected to the MCU domain is different from the EVM board, what modifications are needed?
  2. If the MCU_OSPI[] interface for NOR Flash changes in the MCU domain, what modifications are needed?
  3. How should the EEPROM connected to MCU_I2C0 in the MCU domain be configured?
  4. Can the I2C/SPI resources from the main domain be used in the MCU domain? What documentation provides guidance on this, and could you give an example of how to use the main domain's I2C in the MCU domain?