Part Number: AM4376
Tool/software:
Hi,
I am working on an AM4376-based system and have successfully implemented Spanning Tree Protocol (STP). However, when attempting to enable Rapid Spanning Tree Protocol (RSTP), I am encountering issues.
- Both Ethernet ports on the AM4376 are not functioning correctly in RSTP mode.
- BPDU traffic analysis reveals that no BPDUs are being received or transmitted.
- I have verified the basic Ethernet functionality and STP operation on the board.
- Double-checked the hardware connections for the Ethernet ports.
- Examined the RSTP configuration parameters in the software.
And Help me to find solutions for these questions:-
- Are there any known limitations or specific considerations for RSTP implementation on the AM4376?
- Could there be any hardware or software conflicts that might be preventing RSTP from functioning correctly?
- Are there any debugging techniques or tools that can help me further investigate the RSTP behavior and identify the root cause of the issue?