Other Parts Discussed in Thread: OMAP-L137, CCSTUDIO
I'm trying to build the flash and boot utilities for the OMAP l137. In particular I want to build the UBL NOR bootloader for the DSP. I have a couple of questions:
1) Is it possible to import the CCS v3.3 OMAP-L137/CCS/UBL_DSP/UBL_NOR.pjt into a newer version of code composer? I've tried this in 4.2.1 but got a bunch of errors (which I unfortunately failed to save to report here.) BTW, the reason I want to use 4.x or greater is that CCS v3.3 is not supported on windows 7, and we have had issues with it.
2) I have loaded this into CCS v3.3, but when I build, I get the following errors:
[start_c674x.asm] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -g -o3 -fr"C:/omapl137-flash-boot-utils-20111028/OMAP-L137/CCS/UBL_DSP/NOR" -fs"C:/omapl137-flash-boot-utils-20111028/OMAP-L137/CCS/UBL_DSP/NOR" -i"C:/omapl137-flash-boot-utils-20111028/OMAP-L137/CCS/UBL_DSP/include" -i"C:/omapl137-flash-boot-utils-20111028/OMAP-L137/CCS/UBL_DSP/../../../Common/arch/arm926ejs/include" -i"C:/omapl137-flash-boot-utils-20111028/OMAP-L137/CCS/UBL_DSP/../../../Common/ubl/include" -i"C:/omapl137-flash-boot-utils-20111028/OMAP-L137/CCS/UBL_DSP/../../../Common/gnu/include" -i"C:/omapl137-flash-boot-utils-20111028/OMAP-L137/CCS/UBL_DSP/../../Common/include" -i"C:/omapl137-flash-boot-utils-20111028/OMAP-L137/CCS/UBL_DSP/../../../Common/include" -i"C:/omapl137-flash-boot-utils-20111028/OMAP-L137/CCS/UBL_DSP/../../../Common/drivers/include" --define="UBL_NOR" --cmd_file="C:/omapl137-flash-boot-utils-20111028/OMAP-L137/CCS/UBL_DSP/devtype.txt" -mv6740 -@"../../../OMAP-L137/CCS/UBL_DSP/Debug.lkf" "start_c674x.asm"
"start_c674x.asm", ERROR! at line 16: [E0800] Instruction invalid for C6700
DINT ; Disable Interrupts, FP1, EP1, cycle 0
"start_c674x.asm", ERROR! at line 31: [E0800] Instruction invalid for C6700
CALLP .S2 _main,B3 ; FP2, EP6, cycle 17
2 Assembly Errors, No Assembly Warnings
Any ideas?
Thanks,
Chris