This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM623: Could the image of SK-AM62B-P1 operate normally on the AM6231 platform?

Part Number: AM623

Tool/software:

Hi Expert,

The EVM soc uses AM6254, and the DTS file uses k3-am625-sk.dts.

The customer's board uses AM6231 and boots from SD

1.

The image can be executed normally in the EVM.

Can image run on am6231 without any modification?

2.

If modifications are needed, how should they be modified?

Thanks

Daniel