Tool/software:
Dear Sir,
Customer did use Single channel LVDS panel and it can display normally in SDK 9.0.
In SDK 10.1, it creates new node for OLDI0 and OLDI1 and customer modify the dtso with same panel parameters works in SDK9.
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/791/lvds_5F00_panel.dtso
Now the panel can see the desktop be displayed out but it become 4 desktops in one display.
It should not be problem in Weston because customer try to use Modetest and the result is same.
It looks panel timing has no problem but the data in Frame Buffer are not rendered correctly.


Could you review the dtso and advise which part need to be modified accordingly?
BR, Rich