This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ethernet PHY support at SDK level for DM8168 DM8148 DaVinci ARM DSP



Can I put any PHY in my hardware design and it will likely be supported by the SDK library because

of mostly standard IEEE registers ?

 

Right now I'm considering those two PHYs chip:

- LSI L-ET1011C2-C-D       -> the one chosen for Netra EVM DM8168 designed by Spectrum Digital

- Vitesse VSC8601XKN    -> compact chip since it use RGMII interface 

 

I plan to use one of those chip at full 1000base-T speed most of the time.

But would requires it to be compatible at 10 and 100 Mbits/s.

 

Should I expect issues in future if I choose Vitesse VSC8601XKN ?

Maybe a few registers are non standard and I would requires to write a few read/write functions myself ?

 

E.g.: for the ACT/LINK LED blinking mode.

 

Any other compatible PHY chip to suggest to avoid issues with current TI SDK for DaVinci?