This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VH-Q1: Can we create multiple parameters of a same node as graph parameters

Part Number: TDA4VH-Q1


Tool/software:

Hi TI,

sdk version: 9.2.0.5

I am creating a tiovx graph and in that I have only node that is a custom object array merge node. This node takes 5 input parameters that are vx_object_array type. The node outputs one merged object array merging all elements of all five object array in this output array.

Now my ques is that can I create these five input parameters as graph parameters?

How the dequeue, enqueue will work for these parameters?

regards,

Lalit