Part Number: PROCESSOR-SDK-AM64X
Other Parts Discussed in Thread: TMDS64EVM
Tool/software:
Hi,
I am using dev board TMDS64EVM without os.
I enabled ECC over ddr and over msram.
1. Is there any overhead when running with ECC enabled? Since 1/9 of the memory is allocated for ECC, does writing data to the remaining 8/9 of the memory impose any processing overhead on the main CPU (e.g., R5F)?
2. If there is an overhead, what would it be?
I am talking about cpu overhead during the write read.
eg: When data is written to DDR, the ECC logic must compute the parity bits, which can add latency. or write to the 1/9 area.
Thanks.