This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

QT+C6RUN lib RUN error



Hi, 

 

  I use EZSDK 05.02.01.59, and the version of C6RUN is 0.98.0.0.

  I made a lib use c6run and it works ok when I called it using cpp on the ARM side.

  Also the QT program has tested on ARM side, worked fine.

  But when I put them together, I got a message "Aborted" when I started the QT application.

  I try to find where the program reached, and I found it stopped  at the first line of QT program

  QApplication a(argc, argv);

 

  I think maybe this is because some  memory problem.

  I found in the C6run config file  

------------------------------------------------------------------------------------------------------------------------------------------------------

config.mak

 

PLATFORM=TI816x

C6RUN_INSTALL_DIR=/media/ezsdk/ezsdk_dm816x-evm_5_02_01_59/component-sources/c6run_0_98_00_00

IPC=syslink

DSPOS=sysbios6

GPPOS=linux

SHAREDMEM=cmem

DSP_REGION_BASE_ADDR=0x96C00000

DSP_REGION_CMEM_SIZE=0x02000000

DSP_REGION_CODE_SIZE=0x01500000

 

------------------------------------------------------------------------------------------------------------------------------------------------------

 Memory configures seems different with the table in this URL http://processors.wiki.ti.com/index.php/EZSDK_Memory_Map

 Is this an error of C6run? How can I fix the memory configs?

 

Any advises will be greatly appreciated.

 

Regards,

Lei