Other Parts Discussed in Thread: SK-AM64B
Tool/software:
Hello,
We are planning to use USB as a backup (secondary) boot option and a USB flash drive to flash the primary memory device – eMMC. Currently, I'm experimenting with the SK-AM64B board, where the primary boot option is the SD card, and the secondary boot option is the USB peripheral. I noticed a minor issue: it takes a long time for the system to start booting from the USB device – between 10 to 16 seconds, depending on the USB drive. Is there a way to accelerate this, or is it hardcoded in the internal ROM firmware, meaning we have to live with it?
Regards,
Peter