Other Parts Discussed in Thread: SYSBIOS
Hello,
I'm doing some testing with MJPEG Decoder on HDVICP2 (v01.00.00)
with the DM816x evaluation module. I have build the test application provided
with the decoder release and run it via JTAG.
When using CCS and JTAG to load the test application to the M3 the
decoding can be done successfully. There is no Linux running on the board at that time.
But when trying to launch the application independently with the
slaveloader application from the Syslink sample, I only get hw fault
interrupts. I have seen this by later connecting M3 with the JTAG. Linux is now running on the board.
This perhaps means that I have not successfully taken some co-processor
out of the reset or some clock signal is missing.
I have tried to power up IVAHD0 co-processor via the code provided by the decoder and it seems
to be working at some level because now when using JTAG connection I
don't need to use GEL-script to power up IVAHD0.
But still without the JTAG program loading I can't get the test
application to work. What might be the problem?
Br,
Erkka