Hi Champs,
in the Navigator UG (SPRUGR9D) page 70 - Rx Flow Register A bit 27-26 is stated that a value of 1 is reserved.
However on page 119 in the example on how to configure the RX flow we state:
config_rx_flow(QMSS_PKTDMA_RX_FLOW_REGION, 0 , 0x040002c8, ....)
With the value 0x040002c8 bit 26 is set to "1". This is reserved if page 70 is correct.
Do we need to correct the example or the register description?
Kind regards,
one and zero