Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Good morning TI,
We are currently working on reducing the power consumption of our custom board, which utilizes the AM62A7 processor.We have investigated deep sleep mode as per the TRM, but even in this mode, the power consumption remains at 0.5W, which is significantly higher than our target of 0.35W.We have already attempted to minimize power consumption by stopping the oscillators that remain active during deep sleep, but this has not yielded any noticeable power reduction.
Furthermore, halting the DDR is not feasible as it would necessitate a full system reboot after waking from deep sleep as much i understood from TRM, which is not acceptable for our camera application.We are seeking guidance on potential strategies to further decrease power consumption below the current deep sleep level of 0.5W.
Any suggestions or recommendations would be greatly appreciated.