Other Parts Discussed in Thread: OMAP3530, TCA6416, LM8323, ADS7846, TSC2007, PCF8574, BQ27000, LM63, LM70, LM73, LM77, LM80, LM83, LM87, LM90, LM92, LM93, LM95241, ADS7828, ADS7871, AMC6821, TMP102, TMP401, TMP421, TPS65010, TWL6030, BQ24022, LP3971, LP3972, TPS65023, TLV320AIC23B, TVP5150, TVP7002, THS7303, LP3944, LP5521, LP5523, DAC124S085
I need some help regarding DVI display.
I have a BB rev C4.
I run angstrom images on my BB and the display is perfect on DVI.
So this proves there is no problem with the hardware ....
But now i need to mainline linux kernel 2.6.38.
I have configured the kernel for the board .
I have configured fb0 and fb1. and also the penguin logo.
The display is coming but it blinks for three or four times then the screen blanks (also the penguin logo)
I am struggling this for couple of weeks now.
If reqd I can attach the config file