Which HDMI in interface chip will likely be supported by the SDK library ?
Right now I'm considering those two HDMI Rx interface chip:
- ITE IT6605
- Silicon Image SII9135
Should I expect issues in future ?
I understand that the ITE6605 has two programming requirements:
- powerup registry settings
- real time frame capture by TI SDK
Maybe a few registers are non standard and I would requires to write a few read/write functions myself ?
Does all features of SII9135 already supported in current TI SDK or future ones ?
Any other HDMI Rx chip to suggest that will likely be supported by TI SDK Video capture ?