Hi,
I would like to ask a question on EVMAM1808.

There are power supplies for USB0 and USB1 in the schematics. In OMAP L138 datasheet SPRS586C, table 2-31 also listed these pins as power supply for USB modules.
If none of USB0 or USB1 is used, could ALL these power supply pins be disconnected?, along with the associated capacitors and filters (capacitor-type, Murata, E3, 36, E5, E7)?
Zheng