Other Parts Discussed in Thread: TVP5146
I'm trying to use a dm355-leopardboard to capture images.
When I execute the capture example from the Video for Linux Two API Specification, it always time's out on the select() call. I'm not sure where to start looking for the cause of this problem. The ccdc and camera are passing registration.
[ 2.020000] vpfe_init [ 2.020000] vpfe-capture: vpss clock vpss_master enabled [ 2.030000] vpfe-capture: vpss clock vpss_slave enabled [ 2.040000] vpfe-capture vpfe-capture: v4l2 device registered [ 2.040000] vpfe-capture vpfe-capture: video device registered [ 2.050000] mt9v113 1-003c: Detected a mt9v113 chip ID 2280 [ 2.170000] mt9v113 1-003c: mt9v113 1-003c decoder driver registered !! [ 2.180000] vpfe-capture vpfe-capture: v4l2 sub device mt9v113 registered [ 2.190000] vpfe_register_ccdc_device: DM355 CCDC [ 2.190000] DM355 CCDC is registered with vpfe.
Furthermore, by inspecting the electrical interface to the camera, I have verified that the camera is transmitting pixel data.
What things would cause select() to timeout? Should I look for something in the drivers?
I'm using kernel version Arago/2.6.31+2.6.32-rc2-r52+gitr. Thanks, David