Tool/software:
Hi experts,
my primary issue was a reproducable timeout when trying to downloading a large file using tftp from AM625 linux user space. Interestingly, this works via an IPv4 connection to the tftp server (my laptop computer), but now I'm trying to do it via an IPv6 link-local connection. Note that my setup uses UDP over IPv6.
When debugging with Wireshark running on the tftp server, I noticed that the download timed out at the time when the checksum of the UDP package sent from AM625 to my laptop, hit zero. (The UDP package contents were some ACK messages with package IDs counting up, hence the UDP checksum counted down from some initial value towards zero.) It seems, that my Laptop discarded the ACK response with UDP checksum 0, as mandated by RFC 2460, which describes UDP over IPv6:
o Unlike IPv4, when UDP packets are originated by an IPv6 node, the UDP checksum is not optional. That is, whenever originating a UDP packet, an IPv6 node must compute a UDP checksum over the packet and the pseudo-header, and, if that computation yields a result of zero, it must be changed to hex FFFF for placement in the UDP header. IPv6 receivers must discard UDP packets containing a zero checksum, and should log the error. [emphasis mine]
Temporarily I could solve the issue with
ethtool --offload eth0 tx off
To verify the issue, I wrote a small python script sending a small certain UDP package, adapted to result in an UDP checksum of zero (with some trial and error).
import socket from time import sleep from itertools import cycle ip6 = "fe80::443a:64c4:2cd8:fd26" dev = "eth0" addr = f"{ip6}%{dev}" port = 8648 family, type_, proto, canonname, sockaddr = socket.getaddrinfo( addr, port, family=socket.AF_INET6, type=socket.SOCK_DGRAM, proto=socket.IPPROTO_UDP, ).pop() sock_send = socket.socket(family=family, type=type_, proto=proto) sock_send.sendto(b"t0z-\r\n", sockaddr) # effects UDP_checksum == 0
Indeed, the Hardware offloading logic seems to handle the zero case incorrectly (it should substitute 0x0000 by 0xffff). Insead, the UDP package got send with UDP checksum zero, as indicated on the receiving side via Wireshark:
Question: Did we miss some configuration of the AM625 hardware, that changes the calculation of the IPv6-UDP-checksum in the special case (0 --> 0xffff)? Or is this a hardware bug, and we must resort to software-calculated UDP-checksums?
Thanks in advance and Best Regards,
Lukas Rauber
Hello Lukas,
Thanks for explaining the details of your debug process. First, we have a couple of questions regarding your test setup:
1. Are you testing this on a custom designed board with AM625 or a TI AM62x SK-EVM?
2. What Linux Processors SDK version are you using?
3. If you are finding this issue due to testing on a custom designed board, are you able to see the same issue on a TI AM62x SK-EVM?
4. What is your test topology? (i.e. Is your AM62x device under test directly connected via eth0 to your Laptop with no switch in between? No other ethernet ports on the AM62x device is connected during the test?)
-Daolin
Hello Daolin,
thank you for your quick response. Regarding your questions:
- Linux TI vendor kernel v6.6.32 (based on TI tag 10.00.08) - U-Boot TI vendor v2024.04 (based on TI tag 10.00.08) - Yocto 5.0.3 (Scarthgap) - Qt 6.6
The device boots from SD Card, since the issue occured during our bootstrapping process (from SD Card to eMMC).
The shell to the AM625 I accessed via UART0, using a USB UART adapter, also connected to my laptop.
Update:
3.) Indeed, the issue can also be found on the TI SK-AM62 with the TI image `tisdk-default-image-am62xx-evm-10.01.10.04.rootfs.wic.xz — 1017665 K`:
Hi Lukas,
>>>3.) Indeed, the issue can also be found on the TI SK-AM62 with the TI image `tisdk-default-image-am62xx-evm-10.01.10.04.rootfs.wic.xz — 1017665 K`:
Thanks for confirming.
Can you share the following? Please do this on the TI SK-AM62 evm as that will be easier for me to look into this issue on my side.
1. Results of "ethtool -k eth0" before and after the "ethtool --offload eth0 tx off"?
2. Results of ethtool -S eth0 before and after the illegal UDP checksum message?
3. When sending the UDP packets, these packets were sent from your host laptop to the AM62x device under test? (i.e. the AM62x is receiving the UDP packets or is it the one sending the UDP packets?)
4. If you sent UDP packets with 0 checksum from your host laptop to the AM62x device under test, do you see issues with the UDP rx checksum offload?
-Daolin
No problemo:
root@am62xx-evm:~# ethtool -k eth0 Features for eth0: rx-checksumming: on tx-checksumming: on tx-checksum-ipv4: off [fixed] tx-checksum-ip-generic: on tx-checksum-ipv6: off [fixed] tx-checksum-fcoe-crc: off [fixed] tx-checksum-sctp: off [fixed] scatter-gather: on tx-scatter-gather: on tx-scatter-gather-fraglist: off [fixed] tcp-segmentation-offload: off tx-tcp-segmentation: off [fixed] tx-tcp-ecn-segmentation: off [fixed] tx-tcp-mangleid-segmentation: off [fixed] tx-tcp6-segmentation: off [fixed] generic-segmentation-offload: on generic-receive-offload: on large-receive-offload: off [fixed] rx-vlan-offload: off [fixed] tx-vlan-offload: off [fixed] ntuple-filters: off [fixed] receive-hashing: off [fixed] highdma: off [fixed] rx-vlan-filter: on [fixed] vlan-challenged: off [fixed] tx-lockless: off [fixed] netns-local: off [fixed] tx-gso-robust: off [fixed] tx-fcoe-segmentation: off [fixed] tx-gre-segmentation: off [fixed] tx-gre-csum-segmentation: off [fixed] tx-ipxip4-segmentation: off [fixed] tx-ipxip6-segmentation: off [fixed] tx-udp_tnl-segmentation: off [fixed] tx-udp_tnl-csum-segmentation: off [fixed] tx-gso-partial: off [fixed] tx-tunnel-remcsum-segmentation: off [fixed] tx-sctp-segmentation: off [fixed] tx-esp-segmentation: off [fixed] tx-udp-segmentation: off [fixed] tx-gso-list: off [fixed] fcoe-mtu: off [fixed] tx-nocache-copy: off loopback: off [fixed] rx-fcs: off [fixed] rx-all: off [fixed] tx-vlan-stag-hw-insert: off [fixed] rx-vlan-stag-hw-parse: off [fixed] rx-vlan-stag-filter: off [fixed] l2-fwd-offload: off [fixed] hw-tc-offload: on esp-hw-offload: off [fixed] esp-tx-csum-hw-offload: off [fixed] rx-udp_tunnel-port-offload: off [fixed] tls-hw-tx-offload: off [fixed] tls-hw-rx-offload: off [fixed] rx-gro-hw: off [fixed] tls-hw-record: off [fixed] rx-gro-list: off macsec-hw-offload: off [fixed] rx-udp-gro-forwarding: off hsr-tag-ins-offload: off [fixed] hsr-tag-rm-offload: off [fixed] hsr-fwd-offload: off [fixed] hsr-dup-offload: off [fixed] root@am62xx-evm:~# ethtool --offload eth0 tx off root@am62xx-evm:~# ethtool -k eth0 Features for eth0: rx-checksumming: on tx-checksumming: off tx-checksum-ipv4: off [fixed] tx-checksum-ip-generic: off tx-checksum-ipv6: off [fixed] tx-checksum-fcoe-crc: off [fixed] tx-checksum-sctp: off [fixed] scatter-gather: on tx-scatter-gather: on tx-scatter-gather-fraglist: off [fixed] tcp-segmentation-offload: off tx-tcp-segmentation: off [fixed] tx-tcp-ecn-segmentation: off [fixed] tx-tcp-mangleid-segmentation: off [fixed] tx-tcp6-segmentation: off [fixed] generic-segmentation-offload: on generic-receive-offload: on large-receive-offload: off [fixed] rx-vlan-offload: off [fixed] tx-vlan-offload: off [fixed] ntuple-filters: off [fixed] receive-hashing: off [fixed] highdma: off [fixed] rx-vlan-filter: on [fixed] vlan-challenged: off [fixed] tx-lockless: off [fixed] netns-local: off [fixed] tx-gso-robust: off [fixed] tx-fcoe-segmentation: off [fixed] tx-gre-segmentation: off [fixed] tx-gre-csum-segmentation: off [fixed] tx-ipxip4-segmentation: off [fixed] tx-ipxip6-segmentation: off [fixed] tx-udp_tnl-segmentation: off [fixed] tx-udp_tnl-csum-segmentation: off [fixed] tx-gso-partial: off [fixed] tx-tunnel-remcsum-segmentation: off [fixed] tx-sctp-segmentation: off [fixed] tx-esp-segmentation: off [fixed] tx-udp-segmentation: off [fixed] tx-gso-list: off [fixed] fcoe-mtu: off [fixed] tx-nocache-copy: off loopback: off [fixed] rx-fcs: off [fixed] rx-all: off [fixed] tx-vlan-stag-hw-insert: off [fixed] rx-vlan-stag-hw-parse: off [fixed] rx-vlan-stag-filter: off [fixed] l2-fwd-offload: off [fixed] hw-tc-offload: on esp-hw-offload: off [fixed] esp-tx-csum-hw-offload: off [fixed] rx-udp_tunnel-port-offload: off [fixed] tls-hw-tx-offload: off [fixed] tls-hw-rx-offload: off [fixed] rx-gro-hw: off [fixed] tls-hw-record: off [fixed] rx-gro-list: off macsec-hw-offload: off [fixed] rx-udp-gro-forwarding: off hsr-tag-ins-offload: off [fixed] hsr-tag-rm-offload: off [fixed] hsr-fwd-offload: off [fixed] hsr-dup-offload: off [fixed] root@am62xx-evm:~#
root@am62xx-evm:~# ethtool -S eth0 NIC statistics: p0_rx_good_frames: 27 p0_rx_broadcast_frames: 6 p0_rx_multicast_frames: 21 p0_rx_crc_errors: 0 p0_rx_oversized_frames: 0 p0_rx_undersized_frames: 0 p0_ale_drop: 0 p0_ale_overrun_drop: 0 p0_rx_octets: 4698 p0_tx_good_frames: 41 p0_tx_broadcast_frames: 24 p0_tx_multicast_frames: 17 p0_tx_octets: 6067 p0_tx_64B_frames: 7 p0_tx_65_to_127B_frames: 38 p0_tx_128_to_255B_frames: 9 p0_tx_256_to_511B_frames: 14 p0_tx_512_to_1023B_frames: 0 p0_tx_1024B_frames: 0 p0_net_octets: 10765 p0_rx_bottom_fifo_drop: 0 p0_rx_port_mask_drop: 0 p0_rx_top_fifo_drop: 0 p0_ale_rate_limit_drop: 0 p0_ale_vid_ingress_drop: 0 p0_ale_da_eq_sa_drop: 0 p0_ale_block_drop: 0 p0_ale_secure_drop: 0 p0_ale_auth_drop: 0 p0_ale_unknown_ucast: 0 p0_ale_unknown_ucast_bytes: 0 p0_ale_unknown_mcast: 0 p0_ale_unknown_mcast_bytes: 0 p0_ale_unknown_bcast: 0 p0_ale_unknown_bcast_bytes: 0 p0_ale_pol_match: 0 p0_ale_pol_match_red: 0 p0_ale_pol_match_yellow: 0 p0_ale_mcast_sa_drop: 0 p0_ale_dual_vlan_drop: 0 p0_ale_len_err_drop: 0 p0_ale_ip_next_hdr_drop: 0 p0_ale_ipv4_frag_drop: 0 p0_tx_mem_protect_err: 0 p0_tx_pri0: 41 p0_tx_pri1: 0 p0_tx_pri2: 0 p0_tx_pri3: 0 p0_tx_pri4: 0 p0_tx_pri5: 0 p0_tx_pri6: 0 p0_tx_pri7: 0 p0_tx_pri0_bcnt: 6067 p0_tx_pri1_bcnt: 0 p0_tx_pri2_bcnt: 0 p0_tx_pri3_bcnt: 0 p0_tx_pri4_bcnt: 0 p0_tx_pri5_bcnt: 0 p0_tx_pri6_bcnt: 0 p0_tx_pri7_bcnt: 0 p0_tx_pri0_drop: 0 p0_tx_pri1_drop: 0 p0_tx_pri2_drop: 0 p0_tx_pri3_drop: 0 p0_tx_pri4_drop: 0 p0_tx_pri5_drop: 0 p0_tx_pri6_drop: 0 p0_tx_pri7_drop: 0 p0_tx_pri0_drop_bcnt: 0 p0_tx_pri1_drop_bcnt: 0 p0_tx_pri2_drop_bcnt: 0 p0_tx_pri3_drop_bcnt: 0 p0_tx_pri4_drop_bcnt: 0 p0_tx_pri5_drop_bcnt: 0 p0_tx_pri6_drop_bcnt: 0 p0_tx_pri7_drop_bcnt: 0 rx_good_frames: 142 rx_broadcast_frames: 24 rx_multicast_frames: 118 rx_pause_frames: 0 rx_crc_errors: 0 rx_align_code_errors: 0 rx_oversized_frames: 0 rx_jabber_frames: 0 rx_undersized_frames: 0 rx_fragments: 0 ale_drop: 101 ale_overrun_drop: 0 rx_octets: 19326 tx_good_frames: 27 tx_broadcast_frames: 6 tx_multicast_frames: 21 tx_pause_frames: 0 tx_deferred_frames: 0 tx_collision_frames: 0 tx_single_coll_frames: 0 tx_mult_coll_frames: 0 tx_excessive_collisions: 0 tx_late_collisions: 0 rx_ipg_error: 0 tx_carrier_sense_errors: 0 tx_octets: 4698 tx_64B_frames: 19 tx_65_to_127B_frames: 90 tx_128_to_255B_frames: 39 tx_256_to_511B_frames: 21 tx_512_to_1023B_frames: 0 tx_1024B_frames: 0 net_octets: 24024 rx_bottom_fifo_drop: 0 rx_port_mask_drop: 101 rx_top_fifo_drop: 0 ale_rate_limit_drop: 0 ale_vid_ingress_drop: 0 ale_da_eq_sa_drop: 0 ale_block_drop: 0 ale_secure_drop: 0 ale_auth_drop: 0 ale_unknown_ucast: 0 ale_unknown_ucast_bytes: 0 ale_unknown_mcast: 118 ale_unknown_mcast_bytes: 14934 ale_unknown_bcast: 24 ale_unknown_bcast_bytes: 4392 ale_pol_match: 0 ale_pol_match_red: 0 ale_pol_match_yellow: 0 ale_mcast_sa_drop: 0 ale_dual_vlan_drop: 0 ale_len_err_drop: 0 ale_ip_next_hdr_drop: 0 ale_ipv4_frag_drop: 0 iet_rx_assembly_err: 0 iet_rx_assembly_ok: 0 iet_rx_smd_err: 0 iet_rx_frag: 0 iet_tx_hold: 0 iet_tx_frag: 0 tx_mem_protect_err: 0 tx_pri0: 27 tx_pri1: 0 tx_pri2: 0 tx_pri3: 0 tx_pri4: 0 tx_pri5: 0 tx_pri6: 0 tx_pri7: 0 tx_pri0_bcnt: 4698 tx_pri1_bcnt: 0 tx_pri2_bcnt: 0 tx_pri3_bcnt: 0 tx_pri4_bcnt: 0 tx_pri5_bcnt: 0 tx_pri6_bcnt: 0 tx_pri7_bcnt: 0 tx_pri0_drop: 0 tx_pri1_drop: 0 tx_pri2_drop: 0 tx_pri3_drop: 0 tx_pri4_drop: 0 tx_pri5_drop: 0 tx_pri6_drop: 0 tx_pri7_drop: 0 tx_pri0_drop_bcnt: 0 tx_pri1_drop_bcnt: 0 tx_pri2_drop_bcnt: 0 tx_pri3_drop_bcnt: 0 tx_pri4_drop_bcnt: 0 tx_pri5_drop_bcnt: 0 tx_pri6_drop_bcnt: 0 tx_pri7_drop_bcnt: 0 root@am62xx-evm:~# python3 udp_chksum.py Enter observed UDP checksum (hex): c282 root@am62xx-evm:~# ethtool -S eth0 NIC statistics: p0_rx_good_frames: 31 p0_rx_broadcast_frames: 6 p0_rx_multicast_frames: 22 p0_rx_crc_errors: 0 p0_rx_oversized_frames: 0 p0_rx_undersized_frames: 0 p0_ale_drop: 0 p0_ale_overrun_drop: 0 p0_rx_octets: 5010 p0_tx_good_frames: 47 p0_tx_broadcast_frames: 25 p0_tx_multicast_frames: 19 p0_tx_octets: 6933 p0_tx_64B_frames: 7 p0_tx_65_to_127B_frames: 47 p0_tx_128_to_255B_frames: 9 p0_tx_256_to_511B_frames: 15 p0_tx_512_to_1023B_frames: 0 p0_tx_1024B_frames: 0 p0_net_octets: 11943 p0_rx_bottom_fifo_drop: 0 p0_rx_port_mask_drop: 0 p0_rx_top_fifo_drop: 0 p0_ale_rate_limit_drop: 0 p0_ale_vid_ingress_drop: 0 p0_ale_da_eq_sa_drop: 0 p0_ale_block_drop: 0 p0_ale_secure_drop: 0 p0_ale_auth_drop: 0 p0_ale_unknown_ucast: 0 p0_ale_unknown_ucast_bytes: 0 p0_ale_unknown_mcast: 0 p0_ale_unknown_mcast_bytes: 0 p0_ale_unknown_bcast: 0 p0_ale_unknown_bcast_bytes: 0 p0_ale_pol_match: 0 p0_ale_pol_match_red: 0 p0_ale_pol_match_yellow: 0 p0_ale_mcast_sa_drop: 0 p0_ale_dual_vlan_drop: 0 p0_ale_len_err_drop: 0 p0_ale_ip_next_hdr_drop: 0 p0_ale_ipv4_frag_drop: 0 p0_tx_mem_protect_err: 0 p0_tx_pri0: 47 p0_tx_pri1: 0 p0_tx_pri2: 0 p0_tx_pri3: 0 p0_tx_pri4: 0 p0_tx_pri5: 0 p0_tx_pri6: 0 p0_tx_pri7: 0 p0_tx_pri0_bcnt: 6933 p0_tx_pri1_bcnt: 0 p0_tx_pri2_bcnt: 0 p0_tx_pri3_bcnt: 0 p0_tx_pri4_bcnt: 0 p0_tx_pri5_bcnt: 0 p0_tx_pri6_bcnt: 0 p0_tx_pri7_bcnt: 0 p0_tx_pri0_drop: 0 p0_tx_pri1_drop: 0 p0_tx_pri2_drop: 0 p0_tx_pri3_drop: 0 p0_tx_pri4_drop: 0 p0_tx_pri5_drop: 0 p0_tx_pri6_drop: 0 p0_tx_pri7_drop: 0 p0_tx_pri0_drop_bcnt: 0 p0_tx_pri1_drop_bcnt: 0 p0_tx_pri2_drop_bcnt: 0 p0_tx_pri3_drop_bcnt: 0 p0_tx_pri4_drop_bcnt: 0 p0_tx_pri5_drop_bcnt: 0 p0_tx_pri6_drop_bcnt: 0 p0_tx_pri7_drop_bcnt: 0 rx_good_frames: 150 rx_broadcast_frames: 25 rx_multicast_frames: 122 rx_pause_frames: 0 rx_crc_errors: 0 rx_align_code_errors: 0 rx_oversized_frames: 0 rx_jabber_frames: 0 rx_undersized_frames: 0 rx_fragments: 0 ale_drop: 103 ale_overrun_drop: 0 rx_octets: 20369 tx_good_frames: 31 tx_broadcast_frames: 6 tx_multicast_frames: 22 tx_pause_frames: 0 tx_deferred_frames: 0 tx_collision_frames: 0 tx_single_coll_frames: 0 tx_mult_coll_frames: 0 tx_excessive_collisions: 0 tx_late_collisions: 0 rx_ipg_error: 0 tx_carrier_sense_errors: 0 tx_octets: 5010 tx_64B_frames: 19 tx_65_to_127B_frames: 101 tx_128_to_255B_frames: 39 tx_256_to_511B_frames: 22 tx_512_to_1023B_frames: 0 tx_1024B_frames: 0 net_octets: 25379 rx_bottom_fifo_drop: 0 rx_port_mask_drop: 103 rx_top_fifo_drop: 0 ale_rate_limit_drop: 0 ale_vid_ingress_drop: 0 ale_da_eq_sa_drop: 0 ale_block_drop: 0 ale_secure_drop: 0 ale_auth_drop: 0 ale_unknown_ucast: 3 ale_unknown_ucast_bytes: 298 ale_unknown_mcast: 122 ale_unknown_mcast_bytes: 15333 ale_unknown_bcast: 25 ale_unknown_bcast_bytes: 4738 ale_pol_match: 0 ale_pol_match_red: 0 ale_pol_match_yellow: 0 ale_mcast_sa_drop: 0 ale_dual_vlan_drop: 0 ale_len_err_drop: 0 ale_ip_next_hdr_drop: 0 ale_ipv4_frag_drop: 0 iet_rx_assembly_err: 0 iet_rx_assembly_ok: 0 iet_rx_smd_err: 0 iet_rx_frag: 0 iet_tx_hold: 0 iet_tx_frag: 0 tx_mem_protect_err: 0 tx_pri0: 31 tx_pri1: 0 tx_pri2: 0 tx_pri3: 0 tx_pri4: 0 tx_pri5: 0 tx_pri6: 0 tx_pri7: 0 tx_pri0_bcnt: 5010 tx_pri1_bcnt: 0 tx_pri2_bcnt: 0 tx_pri3_bcnt: 0 tx_pri4_bcnt: 0 tx_pri5_bcnt: 0 tx_pri6_bcnt: 0 tx_pri7_bcnt: 0 tx_pri0_drop: 0 tx_pri1_drop: 0 tx_pri2_drop: 0 tx_pri3_drop: 0 tx_pri4_drop: 0 tx_pri5_drop: 0 tx_pri6_drop: 0 tx_pri7_drop: 0 tx_pri0_drop_bcnt: 0 tx_pri1_drop_bcnt: 0 tx_pri2_drop_bcnt: 0 tx_pri3_drop_bcnt: 0 tx_pri4_drop_bcnt: 0 tx_pri5_drop_bcnt: 0 tx_pri6_drop_bcnt: 0 tx_pri7_drop_bcnt: 0 root@am62xx-evm:~#
import socket ip6 = "fe80::443a:64c4:2cd8:fd26" dev = "eth0" addr = f"{ip6}%{dev}" port = 8648 family, type_, proto, canonname, sockaddr = socket.getaddrinfo( addr, port, family=socket.AF_INET6, type=socket.SOCK_DGRAM, proto=socket.IPPROTO_UDP, ).pop() sock_send = socket.socket(family=family, type=type_, proto=proto) msg = bytearray(b"\x00\x00\r\n") sock_send.sendto(msg, sockaddr) # check package on the other end (e.g. with wireshark), # and observe the UDP cheksum c = int(input("Enter observed UDP checksum (hex): "), 16) # update msg msg[0] = (c >> 8) msg[1] = c & 0xff # send updated msg sock_send.sendto(msg, sockaddr) # this package has UDP chksum zero.
Hi Lukas,
Thanks once again for sharing these details. I will need some time to look into this internally (discuss internally with some colleagues and to replicate this issue), my plan is to work on this tomorrow and provide an update on Friday.
In the meantime, have you looked into how much the CPU load increases when "ethtool --offload eth0 tx off" is used? As I understand, while the CPU load would increase with the tx-checksum offload disabled, the actual load will not increase by a lot. If the CPU load still meets your requirements, it might be sufficient as a workaround until the root-cause of this issue is tracked down.
-Daolin
Update:
I was able to replicate the same issue using your python script. I will be creating an internal bug ticket on this to get it resolved. My suspicion is that the below part of the CPSW driver is not handling the case of IPv6 UDP transmit checksum being 0x0 and making sure the checksum gets sent as 0xffff. It may take some time for the developer to get a fix for this so feel free to try and modify the CPSW driver (am65-cpsw-nuss.c) yourself to see if you can get the tx offload checksum to work.
Orginal patch that covered tx-checksum-offload: https://git.ti.com/cgit/ti-linux-kernel/ti-linux-kernel/commit/drivers/net/ethernet/ti/am65-cpsw-nuss.c?h=ti-rt-linux-6.6.y&id=93a76530316a3d8cc2d82c3deca48424fee92100
The errata mentioned in this part of the driver seems to only apply to AM65x devices and is not on the errata list for AM62x: https://git.ti.com/cgit/ti-linux-kernel/ti-linux-kernel/tree/drivers/net/ethernet/ti/am65-cpsw-nuss.c?h=ti-rt-linux-6.6.y&id=93a76530316a3d8cc2d82c3deca48424fee92100#n1683
-Daolin
Hi Lukas,
I recently discussed with our internal team and it appears that there is a CHECKSUM_INV bit in the RX Control Data Word 2 register that needs to be enabled to ensure zero checksum value is inverted and sent as 0xFFFF (please see the following in the AM62x TRM).
Note that RX in the TRM here is in the perspective of the CPPI internal port, so from CPU to host port, then from host port to one of the external ports, which essentially is the TX checksum handling.
One suggestion the developer gave is to unconditionally set the CHECKSUM_INV bit for all packets (including UDP and TCP) in the CPSW driver, see below. Please note that doing this will cause even IPv4 packets with a checksum of 0 to invert the checksum to 0xFFFF. For some packets, this inversion should not be done since a zero checksum is valid for TCP over IPv4 and over IPv6, and for UDP over IPv4, but it is invalid for UDP over IPv6.
diff --git a/drivers/net/ethernet/ti/am65-cpsw-nuss.c b/drivers/net/ethernet/ti/am65-cpsw-nuss.c index 3d378920e65c..89329ddbb231 100644 --- a/drivers/net/ethernet/ti/am65-cpsw-nuss.c +++ b/drivers/net/ethernet/ti/am65-cpsw-nuss.c @@ -1745,7 +1745,8 @@ static netdev_tx_t am65_cpsw_nuss_ndo_slave_xmit(struct sk_buff *skb, cs_offset = cs_start + skb->csum_offset; /* HW numerates bytes starting from 1 */ psdata[2] = ((cs_offset + 1) << 24) | - ((cs_start + 1) << 16) | (skb->len - cs_start); + ((cs_start + 1) << 16) | (skb->len - cs_start) + | BIT(15); // BIT(15) enables csum inversion for zero csum dev_dbg(dev, "%s tx psdata:%#x\n", __func__, psdata[2]);
The other option is to determine if a packet is UDP IPv6 and selectively setting the CHECKSUM_INV bit but this will defeat the purpose of offloading the checksum calculation to hardware.
Please let us know what you think.
-Daolin
Hi Daolin,
thank you for the input, your helpful and concise information has been greatly appreciated.
We currently are unsure whether we blunder into a trap at a later stage, if we unconditionally set the CHECKSUM_INV bit, especially for TCP over IPv4 packages. Alas, when disabling checksum calculation offloading, the additional CPU usage does not seem to hinder our system noticeably at all.
So, for now, we will resort to software calculation of the checksum (i.e. disable tx offloading).
iff --git a/linux/drivers/net/ethernet/ti/am65-cpsw-nuss.c b/linux/drivers/net/ethernet/ti/am65-cpsw-nuss.c index 81d48e84234..59502664fa1 100644 --- a/linux/drivers/net/ethernet/ti/am65-cpsw-nuss.c +++ b/linux/drivers/net/ethernet/ti/am65-cpsw-nuss.c @@ -9,6 +9,8 @@ #include <linux/etherdevice.h> #include <linux/if_vlan.h> #include <linux/interrupt.h> +#include <linux/ip.h> +#include <linux/ipv6.h> #include <linux/irqdomain.h> #include <linux/kernel.h> #include <linux/kmemleak.h> @@ -1159,6 +1161,14 @@ static netdev_tx_t am65_cpsw_nuss_ndo_slave_xmit(struct sk_buff *skb, /* HW numerates bytes starting from 1 */ psdata[2] = ((cs_offset + 1) << 24) | ((cs_start + 1) << 16) | (skb->len - cs_start); + /* UDP checksum 0 must be written as 0xFFFF. This is done by setting the CHECKSUM_INV bit. */ + if (skb_headlen(skb) >= skb_transport_offset(skb)) { + if ((skb->protocol == htons(ETH_P_IP) && ip_hdr(skb)->protocol == IPPROTO_UDP) || + (skb->protocol == htons(ETH_P_IPV6) && ipv6_hdr(skb)->nexthdr == IPPROTO_UDP)) + psdata[2] |= 0x8000; // set CHECKSUM_INV bit + } else + dev_dbg(dev, "SKB header fragmented!\n"); + dev_dbg(dev, "%s tx psdata:%#x\n", __func__, psdata[2]); }
That is what we use. I was too lazy yet to upstream it.
Hi Ronald,
Thanks for sharing your patch in this thread!
It appears that your patch implements a check for UDP IPv6 and selectively sets the CHECKSUM_INV bit.
As a side note to future readers (and mentioned earlier), this defeats the purpose of offloading checksum calculation to hardware, since we now have the overhead of parsing all packet headers before conditionally setting the 'chksum_inv' bit, so please be aware of this when trying to implement this solution.
-Daolin
The check is only some bytes in the header while the checksum calculation is a bit more expensive because it has to sum up all the data in the packet. So I'm not sure whether this completely defeats the hardware checksum calculation. Do I misunderstand something?
>>>So I'm not sure whether this completely defeats the hardware checksum calculation. Do I misunderstand something?
The note about defeating the purpose of offloading checksum calculation was something that our developer shared with me when I discussed this topic internally. You bring up a good point in that checking the header is only a couple bytes as compared to checksum calculation of all the bytes in the packet. My guess is that our developer meant that simply the action of parsing ALL packets that are meant to be transmitted could take enough load that it offsets any load reduction that checksum offloading would provide. This could be likely considering that, from my understanding, without checksum offload, the actual load would not increase a lot (in other words, with checksum offload, the load benefits would not be by a lot).
Still, it might be worth measuring the load to see if this is actually the case (if CPU load is a concern) since all of this that I described is currently speculative.
-Daolin
There is actually no parsing of the header necessary. The skb data is mapped in memory and the offsets of the bytes to check are known. You need not to be a genius to see that doing the check of some bytes in compare to loading and summing the whole payload is a huge difference. Whether it really matters in the end is another question. For normal use cases it is likely negligible but the kernel should not make assumptions on this. If I find some time I will make some measurements. I will upstream the patch anyway and it will likely get some review by TI people then.