This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 HD_VENC VOUT1 function



HI,

Our customer need to change VOUT1 output form HDMI(default) to DVO1(they connect to VGA).

How to configure this setting?

 

Thanks a lot!!

Shine

  • Hi,

    Following needs to be done

     

    1. You have to setup the pin mux for DVO1. This you can find from pin muxing utility.

    2. You dont have to load ti81xxhdmi.ko module.

    3. you need to set timings using same sysfs entries as you were using earlier.

    Additionally you have to make sure your exteranal DAC is also configured properly.

     

    Regards,

    Hardik Shah

  • Hi HardiShah

    I'm working with the dm8168 and trying to do something similar to what was mentioned above.

    1. I believe I set my DVO1 pin mux values correct.  I did this inside devices.c under ti81xx_video_mux. 

    2. inside the kernel i disabled the hdmi driver.  I believe it's gone since i do a find -name ti81xxhdmi and it's gone.

    3. so the timing signals I'm assuming stay the same in the vpss directory since vout1 is the same as hdmi.

    Lastly i'm not too sure what these dac values are supposed to be set to.  I think that is the only step missing but maybe something above is incorrect.

    Please give me some suggestions i may be able to try to solve this problem.

    Thanks,

    Rodrigo

  • Hi,

    Which PSP release are you using. Can you please dump output

    cat /sys/devices/platform/vpss/display0/output

    I think you have configured Venc for embedded sync and your external decoder/LCD is for discrete sync.   Dumping above output will clear out  things.

    Regards,

    Hardik Shah

  • Hi,

    I have dumped the file and this is what i got.

    / # cat sys/devices/platform/vpss/display0/output
    triplediscrete,rgb888,0/0/0/0
    Our fpga is expecting ycbcr 4:2:2.  
    Rodrigo
  • Sorry just realized I didn't answer the first part of your question.  We are using psp 04.00.01.13

    Rodrigo

  • Rodrigo,

    1. please make sure that pin mux setting do take effect.  M3 firmware may overwrite the DVO1 pinmux.

    2. you can change the VENC output to yuv422

    echo 0 > /sys/devices/platform/vpss/display0/enabled

    echo double/doublediscreted,yuv422spuv > /sys/devices/platform/vpss/display0/enabled

    echo 1 > /sys/devices/platform/vpss/display0/enabled

    Regards

    yihe

  • Thanks for the reply.  The documentation for the vpss driver explained all about the output format but it took me a while to figure out how to determine what the pin mux values are set to.  Finally figure it out and noticed that they have indeed been overwritten.  I've been trying to find where this m3 firmware is overwriting the values i set but can't seem to locate it.  Can you tell me where I should be looking?

    Thanks,

    Rodrigo

  • Rodrigo,

    This is a known issue of the M3 firmware, you can not see it since it is black box. but you can workaround this issue by reconfiguring the pin after loading M3 firmware.

    We are working on fix this for the future release

    Hope this answers your questions.

    Regards,

    yihe

  • Thanks Yihe,

    I'm not too sure where the M3 firmware gets loaded so I've been trying to set the pin mux values on the kernel command line but in doing so my device won't even boot.  Where would be a good place to set the values?

    Thanks,

    Rodrigo

  • Rodrigo,

    M3 firmware is something call ti816x_hdvpss.xem3(PSP) or dm816x_hdvpss.xem3(EZSDK). you can search your file system to see where it is loaded.

    do you use PSP directly or use EZSDK? if using PSP only, you can move to PSP 04.00.02.14 or newer release, m3 firmware does not configure the pinmux.

    if using EZSDK, you can easily add the pin mux codes into your own kernel module(must be dynamitcally) and load this module after M3 firmware is loaded. For example, if you have kernel module to control the external video device connected to VOUT1, please add the pin mux into that driver.

    Regards

    yihe

     

  • Hi,

    Small correction,

    echo 0 > /sys/devices/platform/vpss/display0/enabled

    echo double/doublediscreted,yuv422spuv > /sys/devices/platform/vpss/display0/enabled

    echo 1 > /sys/devices/platform/vpss/display0/enabled

    d is by mistake in above command.

    Regards,

    Hardik Shah