i want to know:
1、i boot the target from nfs, but can't load firmware2. the error is:
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
2、is there source code that can implement streaming media? if not, can i use live555 to implement it?
3、to encode,which module should i use?codec engine、omx、c6accel?
4、to transport the encoded video,which module should i use?